<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC5534 MCU-Boot</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5534-MCU-Boot/m-p/1538356#M50422</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;The MCU-boot is inside&amp;nbsp; Boot ROM:&lt;/P&gt;
&lt;P&gt;192 KB on-chip boot ROM with bootloader that allows various boot options and APIs:&lt;BR /&gt;• Based on ISP pins or CMPA setting in PFR region, supports automated booting from internal flash.&lt;/P&gt;
&lt;P&gt;About detail, you can refer to&amp;nbsp;Chapter 26Boot ROM of lpc554x User Manual.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
    <pubDate>Mon, 17 Oct 2022 07:10:26 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2022-10-17T07:10:26Z</dc:date>
    <item>
      <title>LPC5534 MCU-Boot</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5534-MCU-Boot/m-p/1537994#M50414</link>
      <description>&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;Is there a version of MCU-Boot available for the LPC5534?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
      <pubDate>Fri, 14 Oct 2022 18:26:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5534-MCU-Boot/m-p/1537994#M50414</guid>
      <dc:creator>mjosborne1</dc:creator>
      <dc:date>2022-10-14T18:26:11Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5534 MCU-Boot</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5534-MCU-Boot/m-p/1538356#M50422</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;The MCU-boot is inside&amp;nbsp; Boot ROM:&lt;/P&gt;
&lt;P&gt;192 KB on-chip boot ROM with bootloader that allows various boot options and APIs:&lt;BR /&gt;• Based on ISP pins or CMPA setting in PFR region, supports automated booting from internal flash.&lt;/P&gt;
&lt;P&gt;About detail, you can refer to&amp;nbsp;Chapter 26Boot ROM of lpc554x User Manual.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Mon, 17 Oct 2022 07:10:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5534-MCU-Boot/m-p/1538356#M50422</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2022-10-17T07:10:26Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5534 MCU-Boot</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5534-MCU-Boot/m-p/1538631#M50427</link>
      <description>&lt;P&gt;Hi Alice,&lt;/P&gt;&lt;P&gt;yes I understand that MCU-Boot is the ISP implementation in the LPC5534 ROM; I need a version of the MCU-Boot source code for the LPC5534 .&lt;/P&gt;&lt;P&gt;I'm porting an existing product based on the KL32 to the LPC5534 ; the existing product uses several MCU-Boot based loaders for production and ISP, and I need to update these to support the LPC5534 as well.&lt;/P&gt;&lt;P&gt;As you mentioned, MCU-Boot is the ROM ISP implementation on the LPC5534, so it must have been ported to the LPC5534 right?&amp;nbsp; However, I was unable to find this source code on the site in the part Downloads or in the SDK builder.&lt;/P&gt;&lt;P&gt;We are using the LPC5543 as a recommended alternative due to KL32 availability, so we would greatly appreciate help obtaining a version of MCU-Boot source code for the LPC5543 part, to make this transition easier.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Mon, 17 Oct 2022 14:30:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5534-MCU-Boot/m-p/1538631#M50427</guid>
      <dc:creator>mjosborne1</dc:creator>
      <dc:date>2022-10-17T14:30:25Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5534 MCU-Boot</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5534-MCU-Boot/m-p/1541721#M50466</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/73829"&gt;@mjosborne1&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Sorry the code in MCU-boot is not open source, not public.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Fri, 21 Oct 2022 07:09:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5534-MCU-Boot/m-p/1541721#M50466</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2022-10-21T07:09:36Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5534 MCU-Boot</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5534-MCU-Boot/m-p/1660918#M52808</link>
      <description>&lt;P&gt;Hmm. It can be included when building the SDKs and is available on the site:&amp;nbsp;&lt;A href="https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcu-bootloader-for-nxp-microcontrollers:MCUBOOT" target="_blank"&gt;https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcu-bootloader-for-nxp-microcontrollers:MCUBOOT&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I was just looking for an updated version that included the LPC; we ended up porting it from the K32 to the LPC on our own.&lt;/P&gt;</description>
      <pubDate>Wed, 31 May 2023 15:14:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5534-MCU-Boot/m-p/1660918#M52808</guid>
      <dc:creator>mjosborne1</dc:creator>
      <dc:date>2023-05-31T15:14:20Z</dc:date>
    </item>
  </channel>
</rss>