<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC5526JBD100 ADC pins in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5526JBD100-ADC-pins/m-p/1537651#M50406</link>
    <description>&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;I'm developing a project with LPC5526JBD100 CPU that has to handle ten analog input,&lt;/P&gt;&lt;P&gt;I used all analog inputs assigned to the pins 10,11,12,13,14,20,21,22,23,24&lt;/P&gt;&lt;P&gt;Infortunately pins 12 and 13 conflict width SWD debug pins (SWDIO pin 12 and SWCLK pin 13)&lt;/P&gt;&lt;P&gt;Did you have any similar problem ? How did you fix it?&lt;/P&gt;&lt;P&gt;Thank you very much for your help and cooperation&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;</description>
    <pubDate>Fri, 14 Oct 2022 07:54:12 GMT</pubDate>
    <dc:creator>_Ferrari_</dc:creator>
    <dc:date>2022-10-14T07:54:12Z</dc:date>
    <item>
      <title>LPC5526JBD100 ADC pins</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5526JBD100-ADC-pins/m-p/1537651#M50406</link>
      <description>&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;I'm developing a project with LPC5526JBD100 CPU that has to handle ten analog input,&lt;/P&gt;&lt;P&gt;I used all analog inputs assigned to the pins 10,11,12,13,14,20,21,22,23,24&lt;/P&gt;&lt;P&gt;Infortunately pins 12 and 13 conflict width SWD debug pins (SWDIO pin 12 and SWCLK pin 13)&lt;/P&gt;&lt;P&gt;Did you have any similar problem ? How did you fix it?&lt;/P&gt;&lt;P&gt;Thank you very much for your help and cooperation&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;</description>
      <pubDate>Fri, 14 Oct 2022 07:54:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5526JBD100-ADC-pins/m-p/1537651#M50406</guid>
      <dc:creator>_Ferrari_</dc:creator>
      <dc:date>2022-10-14T07:54:12Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5526JBD100 ADC pins</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5526JBD100-ADC-pins/m-p/1537979#M50412</link>
      <description>&lt;P class="lia-align-justify"&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/202847"&gt;@_Ferrari_&lt;/a&gt;,&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Yes, as you said the LPC5526 needs PIO0_11 and PIO0_12 for SWD operation.&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;You could try to use an extra ADC module (external), for the last two pins that you want to use, and then connect the output to other GPIO pins.&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Hope this helps you.&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Regards, Raul.&lt;/P&gt;</description>
      <pubDate>Fri, 14 Oct 2022 17:26:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5526JBD100-ADC-pins/m-p/1537979#M50412</guid>
      <dc:creator>RaRo</dc:creator>
      <dc:date>2022-10-14T17:26:20Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5526JBD100 ADC pins</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5526JBD100-ADC-pins/m-p/1540920#M50454</link>
      <description>&lt;P&gt;Dear RaulRomero,&lt;/P&gt;&lt;P&gt;thank you for your answer,&lt;/P&gt;&lt;P&gt;you wrote:&lt;/P&gt;&lt;P&gt;&amp;gt;You could try to use an extra ADC module (external), for the last two pins that you want to use, and then connect the output to other GPIO pins&lt;/P&gt;&lt;P&gt;ok, this is the easier solution.&lt;/P&gt;&lt;P&gt;Is there any weakness to use an hardware switch to phisically redirect the pins 12 an 13 to the debugger or to the analog input ?&lt;/P&gt;&lt;P&gt;thank you very much for your help and cooperation.&lt;/P&gt;&lt;P&gt;best regards.&lt;/P&gt;</description>
      <pubDate>Thu, 20 Oct 2022 07:43:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5526JBD100-ADC-pins/m-p/1540920#M50454</guid>
      <dc:creator>_Ferrari_</dc:creator>
      <dc:date>2022-10-20T07:43:17Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5526JBD100 ADC pins</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5526JBD100-ADC-pins/m-p/1540993#M50455</link>
      <description>&lt;P&gt;&lt;EM&gt;&amp;gt; Is there any weakness to use an hardware switch to phisically redirect the pins 12 an 13 to the debugger or to the analog input ?&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Yes.&lt;BR /&gt;You will be unable to debug once the pins are re-initialized by your code.&lt;BR /&gt;Forgoing the debug capability created considerable headaches for many developers trying this approach, just check out this and similar fora.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Since your question suggests you are not very experienced, I would recommend against it.&lt;BR /&gt;Unless you need analogue data rates in the MSps range, an external ADC with serial interface reduces not only the MCU pin count, but also eases the hardware/PCB design, especially in regard to the analog power supply and EMI.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 20 Oct 2022 08:32:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5526JBD100-ADC-pins/m-p/1540993#M50455</guid>
      <dc:creator>frank_m</dc:creator>
      <dc:date>2022-10-20T08:32:50Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5526JBD100 ADC pins</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5526JBD100-ADC-pins/m-p/1541031#M50456</link>
      <description>&lt;P&gt;thanks&lt;/P&gt;&lt;P&gt;Ok&lt;/P&gt;</description>
      <pubDate>Thu, 20 Oct 2022 09:11:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5526JBD100-ADC-pins/m-p/1541031#M50456</guid>
      <dc:creator>_Ferrari_</dc:creator>
      <dc:date>2022-10-20T09:11:41Z</dc:date>
    </item>
  </channel>
</rss>