<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC55S28 SC/PWM Dead-Time and complementary mode in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-SC-PWM-Dead-Time-and-complementary-mode/m-p/1535929#M50378</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Regarding your question, I have to say that the CTimer module does not support complementary PWM signals, in other words, the CTimer match channels can not output complementary PWM signal pair.&lt;/P&gt;
&lt;P&gt;Of course, you can use SCTimer/PWM module to output complementary PWM pair with programmable dead time, but there is not a deadTime register, we set the different match register to implement the complementary PWM pair output.&lt;/P&gt;
&lt;P&gt;Pls refer to section 9. PWM with deadtime in the an11538.pdf, which can be downloaded from the NXP home page:&lt;/P&gt;
&lt;P&gt;You can download the an11538.pdf and the correspond code by searching it in&lt;/P&gt;
&lt;P&gt;&lt;A href="http://www.nxp.com" target="_blank"&gt;www.nxp.com&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
    <pubDate>Wed, 12 Oct 2022 02:38:55 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2022-10-12T02:38:55Z</dc:date>
    <item>
      <title>LPC55S28 SC/PWM Dead-Time and complementary mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-SC-PWM-Dead-Time-and-complementary-mode/m-p/1535504#M50365</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I need to implement two complementary pwm channels on lpc55s28 and change the dead-time using sc timer or ctimer, however in th UM i didn't find a register to do that and in the SDK there's no examples for that use. Does the LPC55 support that ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;HRABI.&lt;/P&gt;</description>
      <pubDate>Tue, 11 Oct 2022 08:59:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-SC-PWM-Dead-Time-and-complementary-mode/m-p/1535504#M50365</guid>
      <dc:creator>ahmedhrabi</dc:creator>
      <dc:date>2022-10-11T08:59:09Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S28 SC/PWM Dead-Time and complementary mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-SC-PWM-Dead-Time-and-complementary-mode/m-p/1535929#M50378</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Regarding your question, I have to say that the CTimer module does not support complementary PWM signals, in other words, the CTimer match channels can not output complementary PWM signal pair.&lt;/P&gt;
&lt;P&gt;Of course, you can use SCTimer/PWM module to output complementary PWM pair with programmable dead time, but there is not a deadTime register, we set the different match register to implement the complementary PWM pair output.&lt;/P&gt;
&lt;P&gt;Pls refer to section 9. PWM with deadtime in the an11538.pdf, which can be downloaded from the NXP home page:&lt;/P&gt;
&lt;P&gt;You can download the an11538.pdf and the correspond code by searching it in&lt;/P&gt;
&lt;P&gt;&lt;A href="http://www.nxp.com" target="_blank"&gt;www.nxp.com&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Wed, 12 Oct 2022 02:38:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-SC-PWM-Dead-Time-and-complementary-mode/m-p/1535929#M50378</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-10-12T02:38:55Z</dc:date>
    </item>
  </channel>
</rss>