<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Hardfault handler on wakeup in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Hardfault-handler-on-wakeup/m-p/1534654#M50357</link>
    <description>&lt;P&gt;1. We have our hard fault handler in FLASH.&lt;/P&gt;&lt;P&gt;2. We can go to deep sleep (using POWER_EnterDeepSleep()) and wakeup on GPIO transition.&amp;nbsp;&lt;/P&gt;&lt;P&gt;3. The function&amp;nbsp;POWER_EnterDeepSleep() says that the HARD FAULT handler should execute from SRAM. What does that mean? Is it correct? We can wakeup from deep sleep even though our HARD FAULT handler is in FLASH.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 10 Oct 2022 07:22:07 GMT</pubDate>
    <dc:creator>PederMoeller</dc:creator>
    <dc:date>2022-10-10T07:22:07Z</dc:date>
    <item>
      <title>Hardfault handler on wakeup</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Hardfault-handler-on-wakeup/m-p/1533750#M50340</link>
      <description>&lt;P&gt;The power down functions&amp;nbsp;&lt;SPAN&gt;POWER_EnterDeepSleep()/&lt;/SPAN&gt;&lt;SPAN&gt;POWER_EnterPowerDown()/&lt;/SPAN&gt;&lt;SPAN&gt;POWER_EnterDeepPowerDown() in&amp;nbsp;&lt;/SPAN&gt;SDK_2_12_0_LPCXpresso55S28\devices\LPC55S28\drivers\fsl_power.hdevices\LPC55S28\drivers\fsl_power.h all have the comment that&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;SPAN&gt;3 - The HARD FAULT handler should execute from SRAM. (The Hard fault handler should initiate a full chip&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;reset)&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;It seems that wakeup from deep sleep works with the hard fault handler being in FLASH and not in SRAM but maybe it is different for some of the other power down modes?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 07 Oct 2022 07:20:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Hardfault-handler-on-wakeup/m-p/1533750#M50340</guid>
      <dc:creator>PederMoeller</dc:creator>
      <dc:date>2022-10-07T07:20:39Z</dc:date>
    </item>
    <item>
      <title>Re: Hardfault handler on wakeup</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Hardfault-handler-on-wakeup/m-p/1534465#M50352</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;SPAN&gt;PederMoeller,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Could you please share more information about the meaning of "It seems that wakeup from deep sleep works with the hard fault handler being in FLASH and not in SRAM but maybe it is different for some of the other power down modes?"? Thanks!&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Alice&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sun, 09 Oct 2022 09:47:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Hardfault-handler-on-wakeup/m-p/1534465#M50352</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2022-10-09T09:47:06Z</dc:date>
    </item>
    <item>
      <title>Re: Hardfault handler on wakeup</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Hardfault-handler-on-wakeup/m-p/1534654#M50357</link>
      <description>&lt;P&gt;1. We have our hard fault handler in FLASH.&lt;/P&gt;&lt;P&gt;2. We can go to deep sleep (using POWER_EnterDeepSleep()) and wakeup on GPIO transition.&amp;nbsp;&lt;/P&gt;&lt;P&gt;3. The function&amp;nbsp;POWER_EnterDeepSleep() says that the HARD FAULT handler should execute from SRAM. What does that mean? Is it correct? We can wakeup from deep sleep even though our HARD FAULT handler is in FLASH.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 10 Oct 2022 07:22:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Hardfault-handler-on-wakeup/m-p/1534654#M50357</guid>
      <dc:creator>PederMoeller</dc:creator>
      <dc:date>2022-10-10T07:22:07Z</dc:date>
    </item>
    <item>
      <title>Re: Hardfault handler on wakeup</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Hardfault-handler-on-wakeup/m-p/1538461#M50425</link>
      <description>&lt;P&gt;Hello ,&lt;/P&gt;
&lt;P&gt;" After enter deep-sleep mode, the MCU and RAM remained powered, but flash and ROM are shut down. So the code in deep-sleep mode need to execute from RAM.&lt;/P&gt;
&lt;P&gt;In our SDK demo, we used GPIO pin interrupt to wakeup from deep-sleep mode. And the GPIO interrupt is one of the wakeup sources of deep-sleep mode. So after triggering GPIO interrupt, the flash is powered first, and then execute handler from flash.&lt;/P&gt;
&lt;P&gt;But the hardfault signal is not the wakeup source of deep-sleep mode, so we need to execute the hardfault handler from RAM and then reset the chip. "&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Mon, 17 Oct 2022 09:20:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Hardfault-handler-on-wakeup/m-p/1538461#M50425</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2022-10-17T09:20:59Z</dc:date>
    </item>
  </channel>
</rss>