<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC8xx measure bandgap with ADC?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC8xx-measure-bandgap-with-ADC/m-p/1530589#M50310</link>
    <description>&lt;P&gt;Apparently, the LPC845 has a 0.9V bandgap reference, mentioned in the Analog Comparator section of the manual.&amp;nbsp; Is it possible to measure that 0.9V with the ADC?&amp;nbsp; I don't see an option for routing it to an ADC input channel.&lt;/P&gt;&lt;P&gt;I want to be able to measure VCC and apply corrections to ADC measurements (of absolute value, not ratiometric to VCC).&amp;nbsp; I also want to compensate the DAC output value based on VCC value.&lt;/P&gt;&lt;P&gt;I'm coming from the Kinetis KL0x which has this ability.&lt;/P&gt;</description>
    <pubDate>Thu, 29 Sep 2022 15:54:02 GMT</pubDate>
    <dc:creator>phatpaul</dc:creator>
    <dc:date>2022-09-29T15:54:02Z</dc:date>
    <item>
      <title>LPC8xx measure bandgap with ADC?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC8xx-measure-bandgap-with-ADC/m-p/1530589#M50310</link>
      <description>&lt;P&gt;Apparently, the LPC845 has a 0.9V bandgap reference, mentioned in the Analog Comparator section of the manual.&amp;nbsp; Is it possible to measure that 0.9V with the ADC?&amp;nbsp; I don't see an option for routing it to an ADC input channel.&lt;/P&gt;&lt;P&gt;I want to be able to measure VCC and apply corrections to ADC measurements (of absolute value, not ratiometric to VCC).&amp;nbsp; I also want to compensate the DAC output value based on VCC value.&lt;/P&gt;&lt;P&gt;I'm coming from the Kinetis KL0x which has this ability.&lt;/P&gt;</description>
      <pubDate>Thu, 29 Sep 2022 15:54:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC8xx-measure-bandgap-with-ADC/m-p/1530589#M50310</guid>
      <dc:creator>phatpaul</dc:creator>
      <dc:date>2022-09-29T15:54:02Z</dc:date>
    </item>
    <item>
      <title>Re: LPC8xx measure bandgap with ADC?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC8xx-measure-bandgap-with-ADC/m-p/1534072#M50351</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/104815"&gt;@phatpaul&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;You are right, there is not an option for routing the 0.9V bandgap reference to an ADC input channel.&lt;/P&gt;
&lt;P&gt;Additionally, you could check this information that could help with your design:&lt;/P&gt;
&lt;UL type="disc"&gt;
&lt;LI&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN5250.pdf" target="_self"&gt;AN5250. How to Increase the Analog-to-Digital Converter Accuracy in an Application&lt;/A&gt;&amp;nbsp;&lt;/LI&gt;
&lt;LI&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN4373.pdf" target="_self"&gt;AN4373. Cookbook for SAR ADC Measurements&lt;/A&gt;&amp;nbsp;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Regards, Raul.&lt;/P&gt;</description>
      <pubDate>Fri, 07 Oct 2022 20:01:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC8xx-measure-bandgap-with-ADC/m-p/1534072#M50351</guid>
      <dc:creator>RaRo</dc:creator>
      <dc:date>2022-10-07T20:01:09Z</dc:date>
    </item>
  </channel>
</rss>