<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Dual Core Release debugging with PE Micro</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Dual-Core-Release-debugging-with-PE-Micro/m-p/1527216#M50250</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Thanks for your sharing.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="VIiyi"&gt;&lt;SPAN class="JLqJ4b ChMk0b"&gt;&lt;SPAN class="Q4iAWc"&gt;It's hard to know exactly where the problem is, and yes, clean and compile is the commonly used method, also can delete folder&amp;nbsp; .metadata under workspace to try.&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="VIiyi"&gt;&lt;SPAN class="JLqJ4b ChMk0b"&gt;&lt;SPAN class="Q4iAWc"&gt;BR&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="VIiyi"&gt;&lt;SPAN class="JLqJ4b ChMk0b"&gt;&lt;SPAN class="Q4iAWc"&gt;Alice&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 23 Sep 2022 08:03:11 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2022-09-23T08:03:11Z</dc:date>
    <item>
      <title>Dual Core Release debugging with PE Micro</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Dual-Core-Release-debugging-with-PE-Micro/m-p/1526080#M50224</link>
      <description>&lt;P&gt;I am using the&amp;nbsp;LPCXPRESSO LPC54102 EVAL BRD (OM13077UL) for developing a dual core project on the LPC54102.&amp;nbsp;I have discovered that when I build my code in Release mode, I am no longer able to use the PE Micro Multi Link probe (connected via SWD)&lt;/P&gt;&lt;P&gt;When I try to launch the debugger, the master image loads fine, but then I get the following error when it tries to load and launch the slave image:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="DanielR_0-1663784435442.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/194526iBB3F9B352D5C471F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="DanielR_0-1663784435442.png" alt="DanielR_0-1663784435442.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;DanielR_0-1663784435442.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The PE Micro probe works in Debug mode and the J Link probe built into the eval board works fine in both Debug and Release mode. This is a problem, because in my final product, I will not have the built in J Link probe, I will only have the SWD port. Is this a limitation of SWD or the PE Micro?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;Daniel&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 21 Sep 2022 18:33:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Dual-Core-Release-debugging-with-PE-Micro/m-p/1526080#M50224</guid>
      <dc:creator>DanielR</dc:creator>
      <dc:date>2022-09-21T18:33:24Z</dc:date>
    </item>
    <item>
      <title>Re: Dual Core Release debugging with PE Micro</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Dual-Core-Release-debugging-with-PE-Micro/m-p/1526814#M50240</link>
      <description>&lt;P&gt;I am not sure what I was doing wrong yesterday. I did a clean and full compile on the Master and Slave and now the PE Micro probe seems to be working fine. I would still like to know what was causing the error yesterday.&lt;/P&gt;</description>
      <pubDate>Thu, 22 Sep 2022 14:31:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Dual-Core-Release-debugging-with-PE-Micro/m-p/1526814#M50240</guid>
      <dc:creator>DanielR</dc:creator>
      <dc:date>2022-09-22T14:31:48Z</dc:date>
    </item>
    <item>
      <title>Re: Dual Core Release debugging with PE Micro</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Dual-Core-Release-debugging-with-PE-Micro/m-p/1527216#M50250</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Thanks for your sharing.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="VIiyi"&gt;&lt;SPAN class="JLqJ4b ChMk0b"&gt;&lt;SPAN class="Q4iAWc"&gt;It's hard to know exactly where the problem is, and yes, clean and compile is the commonly used method, also can delete folder&amp;nbsp; .metadata under workspace to try.&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="VIiyi"&gt;&lt;SPAN class="JLqJ4b ChMk0b"&gt;&lt;SPAN class="Q4iAWc"&gt;BR&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="VIiyi"&gt;&lt;SPAN class="JLqJ4b ChMk0b"&gt;&lt;SPAN class="Q4iAWc"&gt;Alice&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 23 Sep 2022 08:03:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Dual-Core-Release-debugging-with-PE-Micro/m-p/1527216#M50250</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2022-09-23T08:03:11Z</dc:date>
    </item>
  </channel>
</rss>