<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SSP test registers in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/SSP-test-registers/m-p/522384#M5020</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Zoltan on Fri Jun 01 05:46:29 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;As far as I can tell, the SSP on the LPC chips is a standard ARM macrocell.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;However, the NXP docs does not mention the test registers what the ARM docs describe.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;They are extremely handy when you have to run the SSP as a slave. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If you expect to send some data to the master and you load it to the FIFO, then if the master prematurely aborts the transfer your FIFO will not be flushed. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;There is no mechanism to actually FLUSH the FIFO, thus from that point on all frames will be off. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The test registers allow you to actually flush the transmit FIFO in such situations.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I wonder if the test registers are implemented but omitted from the NXP manuals or the test mode is not realised on the silicon at all?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 16:38:59 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T16:38:59Z</dc:date>
    <item>
      <title>SSP test registers</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SSP-test-registers/m-p/522384#M5020</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Zoltan on Fri Jun 01 05:46:29 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;As far as I can tell, the SSP on the LPC chips is a standard ARM macrocell.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;However, the NXP docs does not mention the test registers what the ARM docs describe.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;They are extremely handy when you have to run the SSP as a slave. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If you expect to send some data to the master and you load it to the FIFO, then if the master prematurely aborts the transfer your FIFO will not be flushed. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;There is no mechanism to actually FLUSH the FIFO, thus from that point on all frames will be off. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The test registers allow you to actually flush the transmit FIFO in such situations.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I wonder if the test registers are implemented but omitted from the NXP manuals or the test mode is not realised on the silicon at all?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:38:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SSP-test-registers/m-p/522384#M5020</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:38:59Z</dc:date>
    </item>
    <item>
      <title>Re: SSP test registers</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SSP-test-registers/m-p/522385#M5021</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by DiligentMinds.com on Fri Aug 24 16:07:37 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Perhaps an experiment is in order?&amp;nbsp; When you try it out, please post your results for the rest of us-- along with the code (please)...&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:39:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SSP-test-registers/m-p/522385#M5021</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:39:00Z</dc:date>
    </item>
    <item>
      <title>Re: SSP test registers</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SSP-test-registers/m-p/522386#M5022</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by arshs on Fri Sep 28 09:42:51 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The SSP Test registers are indeed implemented and operational in the LPC (at least in the LPC2300) family, where I have used them for exactly that purpose: clearing the TX/RX FIFOs.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Alex&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:39:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SSP-test-registers/m-p/522386#M5022</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:39:00Z</dc:date>
    </item>
  </channel>
</rss>