<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollersのトピックburning issue with LPC11U68</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/burning-issue-with-LPC11U68/m-p/1521700#M50137</link>
    <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I'm using LPC11U68, I've added some printing with UART to code. After I burned the program to the board at the first UART command I don't see the full buffer transmitted the terminal for example: "ch" is printed instead of "checking".&amp;nbsp;&lt;BR /&gt;The odd thing is when I burned the program on another computer everything works fine, and on a third computer again the some issue as in my computer.&lt;BR /&gt;I even try to reduce the buadrate to 9600 and that didn't solve the issue. In addition I even tried on another board but same issue.&lt;BR /&gt;Someone has an advise how to solve this issue.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
    <pubDate>Wed, 14 Sep 2022 06:16:57 GMT</pubDate>
    <dc:creator>Guy_mego</dc:creator>
    <dc:date>2022-09-14T06:16:57Z</dc:date>
    <item>
      <title>burning issue with LPC11U68</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/burning-issue-with-LPC11U68/m-p/1521700#M50137</link>
      <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I'm using LPC11U68, I've added some printing with UART to code. After I burned the program to the board at the first UART command I don't see the full buffer transmitted the terminal for example: "ch" is printed instead of "checking".&amp;nbsp;&lt;BR /&gt;The odd thing is when I burned the program on another computer everything works fine, and on a third computer again the some issue as in my computer.&lt;BR /&gt;I even try to reduce the buadrate to 9600 and that didn't solve the issue. In addition I even tried on another board but same issue.&lt;BR /&gt;Someone has an advise how to solve this issue.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Wed, 14 Sep 2022 06:16:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/burning-issue-with-LPC11U68/m-p/1521700#M50137</guid>
      <dc:creator>Guy_mego</dc:creator>
      <dc:date>2022-09-14T06:16:57Z</dc:date>
    </item>
    <item>
      <title>Re: burning issue with LPC11U68</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/burning-issue-with-LPC11U68/m-p/1521852#M50142</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I think the uart clock source inaccuracy leads the problem.&lt;/P&gt;
&lt;P&gt;As the following figure for the clock source of LPC51U68, the watchdog oscillator clock frequency is not accurate, I do not think it can be the clock source of uart0. The IRC clock frequency accuracy is +/-1%, I think it is okay for low baudrate. The external 32KHz RTC clock frequency is the most accurate, I suggest you use it as uart clock source.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1663146501760.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/193601i97F614B55EB704DD/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1663146501760.png" alt="xiangjun_rong_0-1663146501760.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 14 Sep 2022 09:16:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/burning-issue-with-LPC11U68/m-p/1521852#M50142</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-09-14T09:16:22Z</dc:date>
    </item>
  </channel>
</rss>