<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックHow can we disable the internal pull-up resistor on a SCT input pin LPC4367</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-can-we-disable-the-internal-pull-up-resistor-on-a-SCT-input/m-p/1521325#M50125</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are currently struggling to disable the internal pull-up resistor on a SCT input pin.&lt;/P&gt;&lt;P&gt;We are using the OM13084 board and the pin we are using is:&lt;/P&gt;&lt;P&gt;Header: J1.19&lt;/P&gt;&lt;P&gt;Pin: P2_6&lt;/P&gt;&lt;P&gt;Function: T3_CAP3&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Where can we set the mode of this pin?&lt;/P&gt;&lt;P&gt;According to UM10503 page 258, the reset state of this pin can either be Neutral or with a pull-up.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;</description>
    <pubDate>Tue, 13 Sep 2022 14:32:55 GMT</pubDate>
    <dc:creator>MariMari</dc:creator>
    <dc:date>2022-09-13T14:32:55Z</dc:date>
    <item>
      <title>How can we disable the internal pull-up resistor on a SCT input pin LPC4367</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-can-we-disable-the-internal-pull-up-resistor-on-a-SCT-input/m-p/1521325#M50125</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are currently struggling to disable the internal pull-up resistor on a SCT input pin.&lt;/P&gt;&lt;P&gt;We are using the OM13084 board and the pin we are using is:&lt;/P&gt;&lt;P&gt;Header: J1.19&lt;/P&gt;&lt;P&gt;Pin: P2_6&lt;/P&gt;&lt;P&gt;Function: T3_CAP3&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Where can we set the mode of this pin?&lt;/P&gt;&lt;P&gt;According to UM10503 page 258, the reset state of this pin can either be Neutral or with a pull-up.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;</description>
      <pubDate>Tue, 13 Sep 2022 14:32:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-can-we-disable-the-internal-pull-up-resistor-on-a-SCT-input/m-p/1521325#M50125</guid>
      <dc:creator>MariMari</dc:creator>
      <dc:date>2022-09-13T14:32:55Z</dc:date>
    </item>
    <item>
      <title>Re: How can we disable the internal pull-up resistor on a SCT input pin LPC4367</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-can-we-disable-the-internal-pull-up-resistor-on-a-SCT-input/m-p/1521435#M50130</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;I found the following information, unfortunately, during the reset state the pull-up can not be disabled, but at the moment the MCU is stable you can disable it with the next register.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Pavel_Hernandez_0-1663099612404.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/193486i5F42246767FB0C97/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Pavel_Hernandez_0-1663099612404.png" alt="Pavel_Hernandez_0-1663099612404.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 13 Sep 2022 20:09:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-can-we-disable-the-internal-pull-up-resistor-on-a-SCT-input/m-p/1521435#M50130</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2022-09-13T20:09:03Z</dc:date>
    </item>
    <item>
      <title>Re: How can we disable the internal pull-up resistor on a SCT input pin LPC4367</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-can-we-disable-the-internal-pull-up-resistor-on-a-SCT-input/m-p/1522632#M50157</link>
      <description>&lt;P&gt;Dear Pavel,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you, we managed to disable the pull-up resistor.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 15 Sep 2022 06:52:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-can-we-disable-the-internal-pull-up-resistor-on-a-SCT-input/m-p/1522632#M50157</guid>
      <dc:creator>MariMari</dc:creator>
      <dc:date>2022-09-15T06:52:49Z</dc:date>
    </item>
  </channel>
</rss>