<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: j-lite cant identify LPC1788 and talk to it</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/j-lite-cant-identify-LPC1788-and-talk-to-it/m-p/522369#M5005</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Haldor on Thu Aug 16 09:24:05 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Answered my own question.&amp;nbsp; FDI has the 20 pin J-Tag to 2mm 10 Pin adapter and you can order it from Digikey.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.digikey.com%2Fproduct-detail%2Fen%2FJLINK-ARM-AD%2F622-1039-ND%2F2631978" rel="nofollow" target="_blank"&gt;http://www.digikey.com/product-detail/en/JLINK-ARM-AD/622-1039-ND/2631978&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:57:25 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:57:25Z</dc:date>
    <item>
      <title>j-lite cant identify LPC1788 and talk to it</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/j-lite-cant-identify-LPC1788-and-talk-to-it/m-p/522366#M5002</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by siriasis on Tue Jan 24 16:39:17 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi Guys. We have recently purchased two kits: uEZGUI-1788-43WQS from FDI one after another and they both stopped working after a few debug sessions with Crossworks IDE. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The JTAG(segger j-lite) that is included in the kit can’t talk anymore to NXP chips on these boards. Below is the screen shot of the J-link commander output.&amp;nbsp; I don’t know what could cause the problem. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;SEGGER J-Link Commander V4.41e ('?' for help) Compiled Jan 19 2012 16:21:49 DLL version V4.41e, compiled Jan 19 2012 16:21:29&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Firmware: J-Link ARM Lite V8 compiled Jan 12 2012 20:49:19&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Hardware: V8.00&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;S/N: 228002481&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;VTarget = 3.313V&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Info: TotalIRLen = ?, IRPrint = 0x..000000000000000000000000 No devices found on JTAG chain. Trying to find device on SWD.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;No device found on SWD.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Did not find any core.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Info: TotalIRLen = ?, IRPrint = 0x..000000000000000000000000 No devices found on JTAG chain. Trying to find device on SWD.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;No device found on SWD.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Did not find any core.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;J-Link&amp;gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I checked the JTAG pins: they are all fine. even something is present on a TDO(data from the CPU) line when the connection is being established. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;At first, when the first kit was killed we thought about static. But when the second board was killed while I was wearing an antistatic strap we started to have some doubts that it happens due to a static. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have also noticed that the second time it stopped working when I plugged the USB cable to the on-board USB connector. The board is powered from this connector. We checked the suppressor U6 connections(may be 5 volt intput on a USB&amp;nbsp; was not properly suppressed) but they were normal.&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;We are now making a flash programmer to check whether the cpu is dead or alive. We are going to perform a whole erase with the help of flash magic tool and a programmer. Perhaps the CPU was locked somehow(CRP1 bit is set). This is also a mystery what could cause the CPU to lock. What do you think about it? &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Guy did anyone work with these kits before. Did you have the same problems. Do you know what can cause it? &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you for your help&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:57:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/j-lite-cant-identify-LPC1788-and-talk-to-it/m-p/522366#M5002</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:57:22Z</dc:date>
    </item>
    <item>
      <title>Re: j-lite cant identify LPC1788 and talk to it</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/j-lite-cant-identify-LPC1788-and-talk-to-it/m-p/522367#M5003</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by usb10185 on Thu Feb 23 09:53:38 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;A few suggestions.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;You can use Flashmagic to check and clear the CRP level if it is lower than CRP3.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Try the JLINK with another target to ensure it is working.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:57:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/j-lite-cant-identify-LPC1788-and-talk-to-it/m-p/522367#M5003</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:57:23Z</dc:date>
    </item>
    <item>
      <title>Re: j-lite cant identify LPC1788 and talk to it</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/j-lite-cant-identify-LPC1788-and-talk-to-it/m-p/522368#M5004</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Haldor on Thu Aug 16 09:17:52 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have used the FDI uEZGUI-1788-43WQS kit successfully.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The problem is with the J-Link Lite LPC edition debugger.&amp;nbsp; It works fine with ARM7 NXP processors, but it is too slow to debug Cortex M3 processors.&amp;nbsp; You can use the LPC edition to download programs to the LPC1788, but even that is not a sure thing. Depending on what I am doing with the LPC1788 I have had problems that required me to disconnect the J-Link Lite LPC debugger from the development board after downloading and then power the development board down and back up before the program started running properly.&amp;nbsp; A bit of a pain, but hey, we all really prefer to debug with printf statements, right?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;P.S. I have never had a Cortex M3 board damaged by the J-Link Lite LPC edition, it simply doesn't support debugging with them.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I just bought a Segger J-Link (the $300 version) and found out that the J-Link Lite LPC edition also used a non-standard JTAG cable (probably because it was designed before the 9 Pin Cortex M3 standard).&amp;nbsp; I purchased the Cortex M3 9 pin adapter from Seggar only to find out that while it is pinned out the same as the J-Link Lite LPC edition, it uses a 2mm connector instead of the 0.05" connector used by the Cortex M3 9 pin connector.&amp;nbsp; Argg.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am looking to see if NXP or FDI has an adapter cable, but if they don't then I will need to fabricate my own.&amp;nbsp; I do wish Segger would offer that adapter since they are still selling the J-Link Lite LPC debugger.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Does anyone know if there is a commercially available adapter to go from the standard 20 pin 0.1" JTAG to the 10 pin 2mm connector used by the J-link Lite LPC edition?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:57:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/j-lite-cant-identify-LPC1788-and-talk-to-it/m-p/522368#M5004</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:57:24Z</dc:date>
    </item>
    <item>
      <title>Re: j-lite cant identify LPC1788 and talk to it</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/j-lite-cant-identify-LPC1788-and-talk-to-it/m-p/522369#M5005</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Haldor on Thu Aug 16 09:24:05 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Answered my own question.&amp;nbsp; FDI has the 20 pin J-Tag to 2mm 10 Pin adapter and you can order it from Digikey.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.digikey.com%2Fproduct-detail%2Fen%2FJLINK-ARM-AD%2F622-1039-ND%2F2631978" rel="nofollow" target="_blank"&gt;http://www.digikey.com/product-detail/en/JLINK-ARM-AD/622-1039-ND/2631978&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:57:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/j-lite-cant-identify-LPC1788-and-talk-to-it/m-p/522369#M5005</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:57:25Z</dc:date>
    </item>
    <item>
      <title>Re: j-lite cant identify LPC1788 and talk to it</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/j-lite-cant-identify-LPC1788-and-talk-to-it/m-p/522370#M5006</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by yuho on Tue Aug 28 04:58:26 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have same problem. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I solved the problem by using FlashMagikTооl. Erasing the chip and it works.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:57:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/j-lite-cant-identify-LPC1788-and-talk-to-it/m-p/522370#M5006</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:57:26Z</dc:date>
    </item>
  </channel>
</rss>