<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic NXP LPC55S36 Secure Boot how to format with SB3.1 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/NXP-LPC55S36-Secure-Boot-how-to-format-with-SB3-1/m-p/1511943#M49962</link>
    <description>&lt;P&gt;Hello All!&lt;/P&gt;&lt;P&gt;I hope all is well.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am working on an LPC55S36 project and I need to boot with Secure Boot. My question is if the SB revokes the internal image for whatever reason, how do I command the LPC to fetch the Golden image formatted with SB3.1 from the external SPI flash? I read the AN 12283 but such information in there.&lt;/P&gt;&lt;P&gt;Also, how do I format my plain image with SB3.1 to be used by the SB?&lt;/P&gt;&lt;P&gt;Thanks much in advance for your help!&lt;/P&gt;</description>
    <pubDate>Thu, 25 Aug 2022 21:27:09 GMT</pubDate>
    <dc:creator>gilmotta2</dc:creator>
    <dc:date>2022-08-25T21:27:09Z</dc:date>
    <item>
      <title>NXP LPC55S36 Secure Boot how to format with SB3.1</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/NXP-LPC55S36-Secure-Boot-how-to-format-with-SB3-1/m-p/1511943#M49962</link>
      <description>&lt;P&gt;Hello All!&lt;/P&gt;&lt;P&gt;I hope all is well.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am working on an LPC55S36 project and I need to boot with Secure Boot. My question is if the SB revokes the internal image for whatever reason, how do I command the LPC to fetch the Golden image formatted with SB3.1 from the external SPI flash? I read the AN 12283 but such information in there.&lt;/P&gt;&lt;P&gt;Also, how do I format my plain image with SB3.1 to be used by the SB?&lt;/P&gt;&lt;P&gt;Thanks much in advance for your help!&lt;/P&gt;</description>
      <pubDate>Thu, 25 Aug 2022 21:27:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/NXP-LPC55S36-Secure-Boot-how-to-format-with-SB3-1/m-p/1511943#M49962</guid>
      <dc:creator>gilmotta2</dc:creator>
      <dc:date>2022-08-25T21:27:09Z</dc:date>
    </item>
    <item>
      <title>Re: NXP LPC55S36 Secure Boot how to format with SB3.1</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/NXP-LPC55S36-Secure-Boot-how-to-format-with-SB3-1/m-p/1512030#M49963</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Can you tell us the part number of LPC family? do you use LPC55S36 exactly?&lt;/P&gt;
&lt;P&gt;As far as I know that LPC55S36 has not been released officially, the current ordering number including the LPC5536-EVK board are LPC5536 instead of LPC55&lt;FONT color="#FF0000"&gt;S&lt;FONT color="#000000"&gt;36, the LPC5536 does not support secure bootloading. Because the LPC5536 does not support secure algorithms such as RSA, hash...&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#FF0000"&gt;&lt;FONT color="#000000"&gt;If you use LPC55S69 or LPC55S69-EVK board, suppose that you can use the dedicated tools: MCUXpresso Secure Provisioning Tool&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#FF0000"&gt;&lt;FONT color="#000000"&gt;which can be downloaded from the link:&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-secure-provisioning-tool:MCUXPRESSO-SECURE-PROVISIONING?tid=vanMCUXPRESSO-SECURE-PROVISIONING" target="_blank"&gt;https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-secure-provisioning-tool:MCUXPRESSO-SECURE-PROVISIONING?tid=vanMCUXPRESSO-SECURE-PROVISIONING&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;You can use the tools to sign a binary file.&lt;/P&gt;
&lt;P&gt;If you are alpha customer and use LPC55S36 exactly which has not been released officially, I am sorry, you can contact local FAE so that they can support you.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#FF0000"&gt;&lt;FONT color="#000000"&gt;LPC55S36 &lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 26 Aug 2022 02:42:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/NXP-LPC55S36-Secure-Boot-how-to-format-with-SB3-1/m-p/1512030#M49963</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-08-26T02:42:51Z</dc:date>
    </item>
  </channel>
</rss>