<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックCan SDA Pin Works if it connected to other GPIO pin which is also pulled up.</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-SDA-Pin-Works-if-it-connected-to-other-GPIO-pin-which-is/m-p/522359#M4995</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by samson.p on Wed Jun 24 03:28:32 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello Everyone,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Am working on&amp;nbsp; LPC1765 controller and am using Analog Sensor and I2C based Color sensor. Both sensors are connected one at a time.We designed in schematic like ADC pin(P0[23]) and SDA pin(P0[27])are joined together through switch&amp;nbsp; when we want to connect I2C based sensor. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;My query is will my I2C sensor will work if i make that ADC pin which was connected to SDA pin as GPIO? &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Kindly support me in this.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Samson &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:56:26 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:56:26Z</dc:date>
    <item>
      <title>Can SDA Pin Works if it connected to other GPIO pin which is also pulled up.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-SDA-Pin-Works-if-it-connected-to-other-GPIO-pin-which-is/m-p/522359#M4995</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by samson.p on Wed Jun 24 03:28:32 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello Everyone,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Am working on&amp;nbsp; LPC1765 controller and am using Analog Sensor and I2C based Color sensor. Both sensors are connected one at a time.We designed in schematic like ADC pin(P0[23]) and SDA pin(P0[27])are joined together through switch&amp;nbsp; when we want to connect I2C based sensor. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;My query is will my I2C sensor will work if i make that ADC pin which was connected to SDA pin as GPIO? &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Kindly support me in this.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Samson &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:56:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-SDA-Pin-Works-if-it-connected-to-other-GPIO-pin-which-is/m-p/522359#M4995</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:56:26Z</dc:date>
    </item>
  </channel>
</rss>