<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックConfig Tools Option for LPC4370</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Config-Tools-Option-for-LPC4370/m-p/1511275#M49946</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am doing a project with the LPC4370 chip. I am wondering if either LPCXpresso or MCUXpresso has the config tools option for it. I have been trying to open up the config tools in MCUXpresso but it's not working since LPC4370 doesn't have SDK package.&lt;BR /&gt;If LPC4370 doesn't have the option for config tools at all, is there a chip that has the same capability of 80MHz data acquisition&amp;nbsp; that has the config tools option?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
    <pubDate>Wed, 24 Aug 2022 22:13:01 GMT</pubDate>
    <dc:creator>mhpham23</dc:creator>
    <dc:date>2022-08-24T22:13:01Z</dc:date>
    <item>
      <title>Config Tools Option for LPC4370</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Config-Tools-Option-for-LPC4370/m-p/1511275#M49946</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am doing a project with the LPC4370 chip. I am wondering if either LPCXpresso or MCUXpresso has the config tools option for it. I have been trying to open up the config tools in MCUXpresso but it's not working since LPC4370 doesn't have SDK package.&lt;BR /&gt;If LPC4370 doesn't have the option for config tools at all, is there a chip that has the same capability of 80MHz data acquisition&amp;nbsp; that has the config tools option?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Wed, 24 Aug 2022 22:13:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Config-Tools-Option-for-LPC4370/m-p/1511275#M49946</guid>
      <dc:creator>mhpham23</dc:creator>
      <dc:date>2022-08-24T22:13:01Z</dc:date>
    </item>
    <item>
      <title>Re: Config Tools Option for LPC4370</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Config-Tools-Option-for-LPC4370/m-p/1511512#M49953</link>
      <description>&lt;P&gt;Hi, Hoan,&lt;/P&gt;
&lt;P&gt;Unfortunately, for LPC43xx, there is not configuration tools to configure the HSADC module of LPC4370. The MCUXpresso tools includes configuration tools, but the tools does not support LPC4370, the LPC4370 is a bit old.&lt;/P&gt;
&lt;P&gt;This is an unofficial code for the HSADC plus DMA, pls refer to it.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Thu, 25 Aug 2022 07:30:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Config-Tools-Option-for-LPC4370/m-p/1511512#M49953</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-08-25T07:30:21Z</dc:date>
    </item>
  </channel>
</rss>