<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC 804 deep power down wakeup is not working</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-804-deep-power-down-wakeup-is-not-working/m-p/1510046#M49933</link>
    <description>&lt;P&gt;Hi&amp;nbsp;RDGC_member&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please note for Deep power-down mode, All clocks, the core, and all peripherals are powered down. Only the WAKEUP pins are powered. All functional pins are tri-stated in deep power-down mode except for the WAKEUP pin.&lt;/P&gt;
&lt;P&gt;Please use WAKEUP pin wake up LPC804 from deep power down mode.&lt;/P&gt;
&lt;P&gt;There is power_mode_switch_lpc demo code under MCUXpresso SDK folder, I suggest you referring it for the low power usage.&lt;/P&gt;
&lt;P&gt;Thanks&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
    <pubDate>Tue, 23 Aug 2022 08:37:45 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2022-08-23T08:37:45Z</dc:date>
    <item>
      <title>LPC 804 deep power down wakeup is not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-804-deep-power-down-wakeup-is-not-working/m-p/1509030#M49912</link>
      <description>&lt;P&gt;We need to use the deep power down mode in our product.&amp;nbsp;&lt;/P&gt;&lt;P&gt;we are successful to put the uc in deep power down mode , also initialized pin PIO0_11 for wake up from deep power down mode .but uc is not waking up. what may be the reason for it .&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;</description>
      <pubDate>Sat, 20 Aug 2022 11:12:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-804-deep-power-down-wakeup-is-not-working/m-p/1509030#M49912</guid>
      <dc:creator>RDGC_member</dc:creator>
      <dc:date>2022-08-20T11:12:09Z</dc:date>
    </item>
    <item>
      <title>Re: LPC 804 deep power down wakeup is not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-804-deep-power-down-wakeup-is-not-working/m-p/1510046#M49933</link>
      <description>&lt;P&gt;Hi&amp;nbsp;RDGC_member&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please note for Deep power-down mode, All clocks, the core, and all peripherals are powered down. Only the WAKEUP pins are powered. All functional pins are tri-stated in deep power-down mode except for the WAKEUP pin.&lt;/P&gt;
&lt;P&gt;Please use WAKEUP pin wake up LPC804 from deep power down mode.&lt;/P&gt;
&lt;P&gt;There is power_mode_switch_lpc demo code under MCUXpresso SDK folder, I suggest you referring it for the low power usage.&lt;/P&gt;
&lt;P&gt;Thanks&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Tue, 23 Aug 2022 08:37:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-804-deep-power-down-wakeup-is-not-working/m-p/1510046#M49933</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2022-08-23T08:37:45Z</dc:date>
    </item>
  </channel>
</rss>