<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: USB Composite device (HID + MSC) - USB stack problem? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-Composite-device-HID-MSC-USB-stack-problem/m-p/1508338#M49878</link>
    <description>&lt;P&gt;can you post the USB trace that exhibits the problem?&lt;/P&gt;</description>
    <pubDate>Thu, 18 Aug 2022 15:33:57 GMT</pubDate>
    <dc:creator>belmontbob59</dc:creator>
    <dc:date>2022-08-18T15:33:57Z</dc:date>
    <item>
      <title>USB Composite device (HID + MSC) - USB stack problem?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-Composite-device-HID-MSC-USB-stack-problem/m-p/1508276#M49876</link>
      <description>&lt;P&gt;I have implemented a &lt;STRONG&gt;HID + MSC&lt;/STRONG&gt; composite USB HS device using the USB stack provided by NXP and starting from the examples.&lt;BR /&gt;- &lt;STRONG&gt;HID&lt;/STRONG&gt;: custom (512byte IN / OUT report on EP1)&lt;BR /&gt;- &lt;STRONG&gt;MSC&lt;/STRONG&gt; with MicroSD support (on EP2)&lt;BR /&gt;I have a fairly serious problem highlighted by USB Analyzer CATC 2500H: almost always the HID transactions are "dirty" or inhibited when an MSC transaction is started at the same time (writing a file on mass storage) and, obviously, the HID part goes into error not completing the transaction.&lt;BR /&gt;It is not the first product of this type that we have developed and this problem was not presented to us.&lt;/P&gt;&lt;P&gt;Do you have any suggestions to fix this?&lt;/P&gt;&lt;P&gt;NOTE&lt;BR /&gt;- Keil SDK&lt;BR /&gt;- No SysOP used&lt;BR /&gt;- NXP 2.12.0 libraries (USB composite - HID - MSC - SD)&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Thu, 18 Aug 2022 13:30:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB-Composite-device-HID-MSC-USB-stack-problem/m-p/1508276#M49876</guid>
      <dc:creator>PaoloS</dc:creator>
      <dc:date>2022-08-18T13:30:47Z</dc:date>
    </item>
    <item>
      <title>Re: USB Composite device (HID + MSC) - USB stack problem?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-Composite-device-HID-MSC-USB-stack-problem/m-p/1508338#M49878</link>
      <description>&lt;P&gt;can you post the USB trace that exhibits the problem?&lt;/P&gt;</description>
      <pubDate>Thu, 18 Aug 2022 15:33:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB-Composite-device-HID-MSC-USB-stack-problem/m-p/1508338#M49878</guid>
      <dc:creator>belmontbob59</dc:creator>
      <dc:date>2022-08-18T15:33:57Z</dc:date>
    </item>
    <item>
      <title>Re: USB Composite device (HID + MSC) - USB stack problem?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-Composite-device-HID-MSC-USB-stack-problem/m-p/1508800#M49895</link>
      <description>&lt;P&gt;&lt;STRONG&gt;SOLVED&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I assumed that the stack would autonomously handle the resending of the &lt;STRONG&gt;HID&lt;/STRONG&gt; packet in the event of a &lt;STRONG&gt;busy pipe&lt;/STRONG&gt;.&lt;BR /&gt;By handling the resend the problem disappeared.&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Thanks anyway for your availability.&lt;/EM&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 19 Aug 2022 13:14:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB-Composite-device-HID-MSC-USB-stack-problem/m-p/1508800#M49895</guid>
      <dc:creator>PaoloS</dc:creator>
      <dc:date>2022-08-19T13:14:43Z</dc:date>
    </item>
  </channel>
</rss>