<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: UM10430 Fan PWM</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/UM10430-Fan-PWM/m-p/1505902#M49839</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I suppose that you use LPC1800 family, it has MotorCONPWM module, you use it to control motor.&lt;/P&gt;
&lt;P&gt;Can you tell us the motor type you are using? do you control BLDC, PMSM or DC motor?&lt;/P&gt;
&lt;P&gt;If you control a DC motor with a bipolar switching mode, it is possible to that you set the PWM duty cycle to zero, the DC motor speed will increase. In the bipolar switching mode&lt;STRONG&gt;,&lt;/STRONG&gt; if you set the duty cycle of PWM in 50%, the DC motor will stall.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 15 Aug 2022 02:23:03 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2022-08-15T02:23:03Z</dc:date>
    <item>
      <title>UM10430 Fan PWM</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/UM10430-Fan-PWM/m-p/1505533#M49834</link>
      <description>&lt;P&gt;When i set the PWM zero it increasing the fanspeed it working fine above 20 pwm .&lt;/P&gt;</description>
      <pubDate>Fri, 12 Aug 2022 10:02:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/UM10430-Fan-PWM/m-p/1505533#M49834</guid>
      <dc:creator>Kushal_Panchal</dc:creator>
      <dc:date>2022-08-12T10:02:10Z</dc:date>
    </item>
    <item>
      <title>Re: UM10430 Fan PWM</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/UM10430-Fan-PWM/m-p/1505902#M49839</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I suppose that you use LPC1800 family, it has MotorCONPWM module, you use it to control motor.&lt;/P&gt;
&lt;P&gt;Can you tell us the motor type you are using? do you control BLDC, PMSM or DC motor?&lt;/P&gt;
&lt;P&gt;If you control a DC motor with a bipolar switching mode, it is possible to that you set the PWM duty cycle to zero, the DC motor speed will increase. In the bipolar switching mode&lt;STRONG&gt;,&lt;/STRONG&gt; if you set the duty cycle of PWM in 50%, the DC motor will stall.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 15 Aug 2022 02:23:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/UM10430-Fan-PWM/m-p/1505902#M49839</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-08-15T02:23:03Z</dc:date>
    </item>
    <item>
      <title>Re: UM10430 Fan PWM</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/UM10430-Fan-PWM/m-p/1509150#M49917</link>
      <description>&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;Yes its help me to resolve my problem.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;kushal&lt;/P&gt;</description>
      <pubDate>Mon, 22 Aug 2022 03:54:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/UM10430-Fan-PWM/m-p/1509150#M49917</guid>
      <dc:creator>Kushal_Panchal</dc:creator>
      <dc:date>2022-08-22T03:54:41Z</dc:date>
    </item>
  </channel>
</rss>