<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Measure USB1_VBUS via internal ADC? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Measure-USB1-VBUS-via-internal-ADC/m-p/1502695#M49799</link>
    <description>&lt;P&gt;Is there a way for the LPC to measure the VBUS voltage via its own ADC?&amp;nbsp;&lt;/P&gt;&lt;P&gt;not sure how the "VBUS_valid" thresholds are measured internally in the chip (or usb phy?)&lt;/P&gt;&lt;P&gt;I found the&amp;nbsp;&lt;SPAN&gt;VBUSVALID_THRESH register, but that doesn't really give me the value of VBUS unless I step through it up and down a few times, not really precise. I'm mainly after being able to read-out a 1-2digit value of what VBUS is at any given time. &lt;EM&gt;(ps. boards already fabbed, and no tap from vbus to an adc input pin)&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 08 Aug 2022 16:11:04 GMT</pubDate>
    <dc:creator>dav1</dc:creator>
    <dc:date>2022-08-08T16:11:04Z</dc:date>
    <item>
      <title>Measure USB1_VBUS via internal ADC?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Measure-USB1-VBUS-via-internal-ADC/m-p/1502695#M49799</link>
      <description>&lt;P&gt;Is there a way for the LPC to measure the VBUS voltage via its own ADC?&amp;nbsp;&lt;/P&gt;&lt;P&gt;not sure how the "VBUS_valid" thresholds are measured internally in the chip (or usb phy?)&lt;/P&gt;&lt;P&gt;I found the&amp;nbsp;&lt;SPAN&gt;VBUSVALID_THRESH register, but that doesn't really give me the value of VBUS unless I step through it up and down a few times, not really precise. I'm mainly after being able to read-out a 1-2digit value of what VBUS is at any given time. &lt;EM&gt;(ps. boards already fabbed, and no tap from vbus to an adc input pin)&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 08 Aug 2022 16:11:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Measure-USB1-VBUS-via-internal-ADC/m-p/1502695#M49799</guid>
      <dc:creator>dav1</dc:creator>
      <dc:date>2022-08-08T16:11:04Z</dc:date>
    </item>
    <item>
      <title>Re: Measure USB1_VBUS via internal ADC?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Measure-USB1-VBUS-via-internal-ADC/m-p/1505497#M49832</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt; VBUS_valid and USB1_VBUS Threshold input level are the same. Regarding VBUS threshold, it depends on if your device is connected to a high-power or a low-power host. for example, In device mode on LPC55, our device tolerance slightly exceeded USB 2.0 spec. requirement, VBUS_valid is 4.192V.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ZhangJennie_0-1660294956346.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/190042iEDAD49CD4B29563F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ZhangJennie_0-1660294956346.png" alt="ZhangJennie_0-1660294956346.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;ZhangJennie_0-1660294956346.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Thus if USB module detects&amp;nbsp;&amp;nbsp;USB1_VBUS&amp;nbsp; is less than 4.192. USB module can't work normally.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Hope this helps，&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Jun Zhang&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 12 Aug 2022 09:02:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Measure-USB1-VBUS-via-internal-ADC/m-p/1505497#M49832</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2022-08-12T09:02:44Z</dc:date>
    </item>
  </channel>
</rss>