<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 NXP RFID-Card RC663 and Distance</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/NXP-RFID-Card-RC663-and-Distance/m-p/522338#M4974</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by t9cpu on Mon Jul 21 00:09:06 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello !&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If this is not the right place sorry... but maybe someone can help me.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have the NXP RC663 RFID Card and the Antenna is now OK. The Smith-Diagramm shows me I'm near the Point 1 and the Swr shows me a relation from 1.1:1. So I think this is OK. To read the UID is no Problem from a distance like 3 cm. But the LPCD-detection is not very well. A distance from 2-3mm is necessary to detect a card. And also not every time a card is detected. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there someone who has experience with it and can help me ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 16:39:51 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T16:39:51Z</dc:date>
    <item>
      <title>NXP RFID-Card RC663 and Distance</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/NXP-RFID-Card-RC663-and-Distance/m-p/522338#M4974</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by t9cpu on Mon Jul 21 00:09:06 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello !&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If this is not the right place sorry... but maybe someone can help me.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have the NXP RC663 RFID Card and the Antenna is now OK. The Smith-Diagramm shows me I'm near the Point 1 and the Swr shows me a relation from 1.1:1. So I think this is OK. To read the UID is no Problem from a distance like 3 cm. But the LPCD-detection is not very well. A distance from 2-3mm is necessary to detect a card. And also not every time a card is detected. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there someone who has experience with it and can help me ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:39:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/NXP-RFID-Card-RC663-and-Distance/m-p/522338#M4974</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:39:51Z</dc:date>
    </item>
    <item>
      <title>Re: NXP RFID-Card RC663 and Distance</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/NXP-RFID-Card-RC663-and-Distance/m-p/522339#M4975</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Sergio29 on Sun Dec 07 23:37:10 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi t9cpu&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;You are right&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Today, always waiting for NXP help and solutions, I think what LPCD function on MFRC630 or CLRC663 NXP Mifare component is virtually unusable for using it in low power with non-rechargeable batteries.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I think it's the only&amp;nbsp; reason to use LPCD function, is'nt it ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;A lot of parameters make it to fail (such has temperature variation)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;6 month ago I start working on those problems and today I haven't found a really good solution.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;I contact NXP via EBV for this problems 5 months ago with all explanations and I have transmit&amp;nbsp;&amp;nbsp; my schematic and board design with only this answer "All works fine, no one experiencing this problem" !!!!!&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;You can just verify this problems with the red evaluation board !&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Sometimes it detect without card presence&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Sometime at 1 cm&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Sometime at 2 cms&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Sometime there is no more detection&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;It's changing day to day.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Try to reduce Rxp ans Rxn resistor in your design, I decrease it from 15k Ohm to 10K or 8K for better results&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;(Always assuming that&amp;nbsp; RXp and RXp does not exceed max level) &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;But variations of card detection stay here...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What board do you use ? &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Can you send to me your documentation if it's your own design board, I will do it too if you want.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If you plan tu use LPCD using non-rechargeable batteries, keep in mind that erronous detection will use&amp;nbsp; 80 to 100 ma on power supply during Request command (40ms) to verify presence of the card !&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have used software solution to resolve this other problem but it's not really the good solution...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Exepted the LPCD function, this component works very fine&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Happy to read you&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Serge&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:39:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/NXP-RFID-Card-RC663-and-Distance/m-p/522339#M4975</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:39:52Z</dc:date>
    </item>
  </channel>
</rss>