<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: No Flash configured</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/No-Flash-configured/m-p/1494863#M49686</link>
    <description>&lt;P&gt;Hi Alice_Yang,&lt;/P&gt;&lt;P&gt;Thank you for your response. I want to download it to the external flash. From the console message that I attached to my first message, it seems that the internal flash could be successfully programmed, but not the external one. Is there any sample project for LPC4088 that I can try to verify the hardware is working and see how to manage it?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Mon, 25 Jul 2022 13:53:14 GMT</pubDate>
    <dc:creator>bamdadslr</dc:creator>
    <dc:date>2022-07-25T13:53:14Z</dc:date>
    <item>
      <title>No Flash configured</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/No-Flash-configured/m-p/1494208#M49674</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to use the MCUXpresso GUI Flash Tool to program a LPC4088 chip with my own code. On the board, there exists an external flash drive of 4MB and I am using the NXP LINK2 CMSIS-DAP debug probe. You can find screenshot of the settings that I have:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Pic1.png" style="width: 422px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/187579iD1168A244752D415/image-dimensions/422x362?v=v2" width="422" height="362" role="button" title="Pic1.png" alt="Pic1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Pic2.png" style="width: 555px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/187580i75FEF7621C110F50/image-dimensions/555x732?v=v2" width="555" height="732" role="button" title="Pic2.png" alt="Pic2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Pic3.png" style="width: 533px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/187581iD2BB46B2527494C3/image-dimensions/533x427?v=v2" width="533" height="427" role="button" title="Pic3.png" alt="Pic3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Now, when I press the run on the flash tool, I get the following error:&lt;BR /&gt;Executing flash operation 'Program' (Program file into flash: TEST3.axf) - Fri Jul 22 14:34:13 CDT 2022&lt;BR /&gt;Checking MCU info...&lt;BR /&gt;Scanning for targets...&lt;BR /&gt;Executing flash action...&lt;BR /&gt;MCUXpresso IDE RedlinkMulti Driver v11.5 (Apr 7 2022 16:04:36 - crt_emu_cm_redlink.exe build 11)&lt;BR /&gt;( 0) Reading remote configuration&lt;BR /&gt;Wc(03). No cache support.&lt;BR /&gt;Found chip XML file in D:/VELOX/Software/3_Coding_WorkSpace/TEST3/Debug\LPC4088.xml&lt;BR /&gt;( 5) Remote configuration complete&lt;BR /&gt;Reconnected to existing LinkServer process.&lt;BR /&gt;Probe Firmware: LPC-LINK2 CMSIS-DAP V5.361 (NXP Semiconductors)&lt;BR /&gt;Serial Number: MSB4IYES&lt;BR /&gt;VID:PID: 1FC9:0090&lt;BR /&gt;USB Path: \\?\hid#vid_1fc9&amp;amp;pid_0090&amp;amp;mi_00#8&amp;amp;23730db6&amp;amp;0&amp;amp;0000#{4d1e55b2-f16f-11cf-88cb-001111000030}&lt;BR /&gt;Using memory from core 0 after searching for a good core&lt;BR /&gt;( 30) Emulator Connected&lt;BR /&gt;( 40) Debug Halt&lt;BR /&gt;( 50) CPU ID&lt;BR /&gt;debug interface type = CoreSight DP (DAP DP ID 2BA01477) over SWD TAP 0&lt;BR /&gt;processor type = Cortex-M4 (CPU ID 00000C24) on DAP AP 0&lt;BR /&gt;number of h/w breakpoints = 6&lt;BR /&gt;number of flash patches = 2&lt;BR /&gt;number of h/w watchpoints = 4&lt;BR /&gt;Probe(0): Connected&amp;amp;Reset. DpID: 2BA01477. CpuID: 00000C24. Info: &amp;lt;None&amp;gt;&lt;BR /&gt;Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.&lt;BR /&gt;Content of CoreSight Debug ROM(s):&lt;BR /&gt;RBASE E00FF000: CID B105100D PID 04000BB4C4 ROM (type 0x1)&lt;BR /&gt;ROM 1 E000E000: CID B105E00D PID 04000BB00C Gen SCS (type 0x0)&lt;BR /&gt;ROM 1 E0001000: CID B105E00D PID 04003BB002 Gen DWT (type 0x0)&lt;BR /&gt;ROM 1 E0002000: CID B105E00D PID 04002BB003 Gen FPB (type 0x0)&lt;BR /&gt;ROM 1 E0000000: CID B105E00D PID 04003BB001 Gen ITM (type 0x0)&lt;BR /&gt;ROM 1 E0040000: CID B105900D PID 04000BB9A1 CSt TPIU type 0x11 Trace Sink - TPIU&lt;BR /&gt;ROM 1 E0041000: CID B105900D PID 04000BB925 CSt ETM type 0x13 Trace Source - Core&lt;BR /&gt;NXP: LPC4088&lt;BR /&gt;DAP stride is 4096 bytes (1024 words)&lt;BR /&gt;Inspected v.2 On-chip Flash Memory LPC177x_8x_407x_8x_512.cfx&lt;BR /&gt;Image 'LPC177x_8x_407x_8x (512K) Apr 11 2022 10:49:09'&lt;BR /&gt;( 65) Chip Setup Complete&lt;BR /&gt;Connected: was_reset=true. was_stopped=false&lt;BR /&gt;( 70) License Check Complete&lt;BR /&gt;Loading 'TEST3.axf' ELF 0x00000000 len 0x7C52C&lt;BR /&gt;Opening flash driver LPC177x_8x_407x_8x_512.cfx&lt;BR /&gt;Sending VECTRESET to run flash driver&lt;BR /&gt;Flash device supported (512KB = 16*4K 14*32K at 0x0)&lt;BR /&gt;Writing 509228 bytes to address 0x00000000 in Flash&lt;BR /&gt;( 0) Mass erasing Flash&lt;BR /&gt;Mass erased flash in 113msec&lt;BR /&gt;1 of 1 ( 0) Writing sectors 0-29 at 0x00000000 with 509228 bytes&lt;BR /&gt;( 0) at 00000000: 0 bytes - 0/509228&lt;BR /&gt;( 0) at 00000000: 4096 bytes - 4096/509228&lt;BR /&gt;( 1) at 00001000: 4096 bytes - 8192/509228&lt;BR /&gt;( 2) at 00002000: 4096 bytes - 12288/509228&lt;BR /&gt;( 3) at 00003000: 4096 bytes - 16384/509228&lt;BR /&gt;( 4) at 00004000: 4096 bytes - 20480/509228&lt;BR /&gt;( 4) at 00005000: 4096 bytes - 24576/509228&lt;BR /&gt;( 5) at 00006000: 4096 bytes - 28672/509228&lt;BR /&gt;( 6) at 00007000: 4096 bytes - 32768/509228&lt;BR /&gt;( 7) at 00008000: 4096 bytes - 36864/509228&lt;BR /&gt;( &lt;LI-EMOJI id="lia_smiling-face-with-sunglasses" title=":smiling_face_with_sunglasses:"&gt;&lt;/LI-EMOJI&gt; at 00009000: 4096 bytes - 40960/509228&lt;BR /&gt;( &lt;LI-EMOJI id="lia_smiling-face-with-sunglasses" title=":smiling_face_with_sunglasses:"&gt;&lt;/LI-EMOJI&gt; at 0000A000: 4096 bytes - 45056/509228&lt;BR /&gt;( 9) at 0000B000: 4096 bytes - 49152/509228&lt;BR /&gt;( 10) at 0000C000: 4096 bytes - 53248/509228&lt;BR /&gt;( 11) at 0000D000: 4096 bytes - 57344/509228&lt;BR /&gt;( 12) at 0000E000: 4096 bytes - 61440/509228&lt;BR /&gt;( 12) at 0000F000: 4096 bytes - 65536/509228&lt;BR /&gt;( 13) at 00010000: 4096 bytes - 69632/509228&lt;BR /&gt;( 14) at 00011000: 4096 bytes - 73728/509228&lt;BR /&gt;( 15) at 00012000: 4096 bytes - 77824/509228&lt;BR /&gt;( 16) at 00013000: 4096 bytes - 81920/509228&lt;BR /&gt;( 16) at 00014000: 4096 bytes - 86016/509228&lt;BR /&gt;( 17) at 00015000: 4096 bytes - 90112/509228&lt;BR /&gt;( 18) at 00016000: 4096 bytes - 94208/509228&lt;BR /&gt;( 19) at 00017000: 4096 bytes - 98304/509228&lt;BR /&gt;( 20) at 00018000: 4096 bytes - 102400/509228&lt;BR /&gt;( 20) at 00019000: 4096 bytes - 106496/509228&lt;BR /&gt;( 21) at 0001A000: 4096 bytes - 110592/509228&lt;BR /&gt;( 22) at 0001B000: 4096 bytes - 114688/509228&lt;BR /&gt;( 23) at 0001C000: 4096 bytes - 118784/509228&lt;BR /&gt;( 24) at 0001D000: 4096 bytes - 122880/509228&lt;BR /&gt;( 24) at 0001E000: 4096 bytes - 126976/509228&lt;BR /&gt;( 25) at 0001F000: 4096 bytes - 131072/509228&lt;BR /&gt;( 26) at 00020000: 4096 bytes - 135168/509228&lt;BR /&gt;( 27) at 00021000: 4096 bytes - 139264/509228&lt;BR /&gt;( 28) at 00022000: 4096 bytes - 143360/509228&lt;BR /&gt;( 28) at 00023000: 4096 bytes - 147456/509228&lt;BR /&gt;( 29) at 00024000: 4096 bytes - 151552/509228&lt;BR /&gt;( 30) at 00025000: 4096 bytes - 155648/509228&lt;BR /&gt;( 31) at 00026000: 4096 bytes - 159744/509228&lt;BR /&gt;( 32) at 00027000: 4096 bytes - 163840/509228&lt;BR /&gt;( 32) at 00028000: 4096 bytes - 167936/509228&lt;BR /&gt;( 33) at 00029000: 4096 bytes - 172032/509228&lt;BR /&gt;( 34) at 0002A000: 4096 bytes - 176128/509228&lt;BR /&gt;( 35) at 0002B000: 4096 bytes - 180224/509228&lt;BR /&gt;( 36) at 0002C000: 4096 bytes - 184320/509228&lt;BR /&gt;( 37) at 0002D000: 4096 bytes - 188416/509228&lt;BR /&gt;( 37) at 0002E000: 4096 bytes - 192512/509228&lt;BR /&gt;( 38) at 0002F000: 4096 bytes - 196608/509228&lt;BR /&gt;( 39) at 00030000: 4096 bytes - 200704/509228&lt;BR /&gt;( 40) at 00031000: 4096 bytes - 204800/509228&lt;BR /&gt;( 41) at 00032000: 4096 bytes - 208896/509228&lt;BR /&gt;( 41) at 00033000: 4096 bytes - 212992/509228&lt;BR /&gt;( 42) at 00034000: 4096 bytes - 217088/509228&lt;BR /&gt;( 43) at 00035000: 4096 bytes - 221184/509228&lt;BR /&gt;( 44) at 00036000: 4096 bytes - 225280/509228&lt;BR /&gt;( 45) at 00037000: 4096 bytes - 229376/509228&lt;BR /&gt;( 45) at 00038000: 4096 bytes - 233472/509228&lt;BR /&gt;( 46) at 00039000: 4096 bytes - 237568/509228&lt;BR /&gt;( 47) at 0003A000: 4096 bytes - 241664/509228&lt;BR /&gt;( 48) at 0003B000: 4096 bytes - 245760/509228&lt;BR /&gt;( 49) at 0003C000: 4096 bytes - 249856/509228&lt;BR /&gt;( 49) at 0003D000: 4096 bytes - 253952/509228&lt;BR /&gt;( 50) at 0003E000: 4096 bytes - 258048/509228&lt;BR /&gt;( 51) at 0003F000: 4096 bytes - 262144/509228&lt;BR /&gt;( 52) at 00040000: 4096 bytes - 266240/509228&lt;BR /&gt;( 53) at 00041000: 4096 bytes - 270336/509228&lt;BR /&gt;( 53) at 00042000: 4096 bytes - 274432/509228&lt;BR /&gt;( 54) at 00043000: 4096 bytes - 278528/509228&lt;BR /&gt;( 55) at 00044000: 4096 bytes - 282624/509228&lt;BR /&gt;( 56) at 00045000: 4096 bytes - 286720/509228&lt;BR /&gt;( 57) at 00046000: 4096 bytes - 290816/509228&lt;BR /&gt;( 57) at 00047000: 4096 bytes - 294912/509228&lt;BR /&gt;( 58) at 00048000: 4096 bytes - 299008/509228&lt;BR /&gt;( 59) at 00049000: 4096 bytes - 303104/509228&lt;BR /&gt;( 60) at 0004A000: 4096 bytes - 307200/509228&lt;BR /&gt;( 61) at 0004B000: 4096 bytes - 311296/509228&lt;BR /&gt;( 61) at 0004C000: 4096 bytes - 315392/509228&lt;BR /&gt;( 62) at 0004D000: 4096 bytes - 319488/509228&lt;BR /&gt;( 63) at 0004E000: 4096 bytes - 323584/509228&lt;BR /&gt;( 64) at 0004F000: 4096 bytes - 327680/509228&lt;BR /&gt;( 65) at 00050000: 4096 bytes - 331776/509228&lt;BR /&gt;( 65) at 00051000: 4096 bytes - 335872/509228&lt;BR /&gt;( 66) at 00052000: 4096 bytes - 339968/509228&lt;BR /&gt;( 67) at 00053000: 4096 bytes - 344064/509228&lt;BR /&gt;( 68) at 00054000: 4096 bytes - 348160/509228&lt;BR /&gt;( 69) at 00055000: 4096 bytes - 352256/509228&lt;BR /&gt;( 69) at 00056000: 4096 bytes - 356352/509228&lt;BR /&gt;( 70) at 00057000: 4096 bytes - 360448/509228&lt;BR /&gt;( 71) at 00058000: 4096 bytes - 364544/509228&lt;BR /&gt;( 72) at 00059000: 4096 bytes - 368640/509228&lt;BR /&gt;( 73) at 0005A000: 4096 bytes - 372736/509228&lt;BR /&gt;( 74) at 0005B000: 4096 bytes - 376832/509228&lt;BR /&gt;( 74) at 0005C000: 4096 bytes - 380928/509228&lt;BR /&gt;( 75) at 0005D000: 4096 bytes - 385024/509228&lt;BR /&gt;( 76) at 0005E000: 4096 bytes - 389120/509228&lt;BR /&gt;( 77) at 0005F000: 4096 bytes - 393216/509228&lt;BR /&gt;( 78) at 00060000: 4096 bytes - 397312/509228&lt;BR /&gt;( 78) at 00061000: 4096 bytes - 401408/509228&lt;BR /&gt;( 79) at 00062000: 4096 bytes - 405504/509228&lt;BR /&gt;( 80) at 00063000: 4096 bytes - 409600/509228&lt;BR /&gt;( 81) at 00064000: 4096 bytes - 413696/509228&lt;BR /&gt;( 82) at 00065000: 4096 bytes - 417792/509228&lt;BR /&gt;( 82) at 00066000: 4096 bytes - 421888/509228&lt;BR /&gt;( 83) at 00067000: 4096 bytes - 425984/509228&lt;BR /&gt;( 84) at 00068000: 4096 bytes - 430080/509228&lt;BR /&gt;( 85) at 00069000: 4096 bytes - 434176/509228&lt;BR /&gt;( 86) at 0006A000: 4096 bytes - 438272/509228&lt;BR /&gt;( 86) at 0006B000: 4096 bytes - 442368/509228&lt;BR /&gt;( 87) at 0006C000: 4096 bytes - 446464/509228&lt;BR /&gt;( 88) at 0006D000: 4096 bytes - 450560/509228&lt;BR /&gt;( 89) at 0006E000: 4096 bytes - 454656/509228&lt;BR /&gt;( 90) at 0006F000: 4096 bytes - 458752/509228&lt;BR /&gt;( 90) at 00070000: 4096 bytes - 462848/509228&lt;BR /&gt;( 91) at 00071000: 4096 bytes - 466944/509228&lt;BR /&gt;( 92) at 00072000: 4096 bytes - 471040/509228&lt;BR /&gt;( 93) at 00073000: 4096 bytes - 475136/509228&lt;BR /&gt;( 94) at 00074000: 4096 bytes - 479232/509228&lt;BR /&gt;( 94) at 00075000: 4096 bytes - 483328/509228&lt;BR /&gt;( 95) at 00076000: 4096 bytes - 487424/509228&lt;BR /&gt;( 96) at 00077000: 4096 bytes - 491520/509228&lt;BR /&gt;( 97) at 00078000: 4096 bytes - 495616/509228&lt;BR /&gt;( 98) at 00079000: 4096 bytes - 499712/509228&lt;BR /&gt;( 98) at 0007A000: 4096 bytes - 503808/509228&lt;BR /&gt;( 99) at 0007B000: 4096 bytes - 507904/509228&lt;BR /&gt;(100) at 0007C000: 4096 bytes - 512000/509228&lt;BR /&gt;Sectors written: 30, unchanged: 0, total: 30&lt;BR /&gt;Wrote sector 0-29 with 509228 bytes in 3906msec&lt;BR /&gt;Closing flash driver LPC177x_8x_407x_8x_512.cfx&lt;BR /&gt;(100) Finished writing Flash successfully.&lt;BR /&gt;Flash Write Done&lt;BR /&gt;Loaded 0x7C52C bytes in 4179ms (about 121kB/s)&lt;BR /&gt;Loading 'TEST3.axf' ELF 0x28000000 len 0x15A1B8&lt;BR /&gt;File 'TEST3.axf' load failure: Ef(11). No flash configured.&lt;BR /&gt;Loading 'TEST3.axf' ELF 0x28200000 len 0x18F290&lt;BR /&gt;File 'TEST3.axf' load failure: Ef(11). No flash configured.&lt;BR /&gt;(100) Target Connection Failed&lt;BR /&gt;Unable to perform operation!&lt;BR /&gt;Command failed with exit code 1&lt;BR /&gt;&lt;BR /&gt;I would appreciate any help.&lt;/P&gt;</description>
      <pubDate>Fri, 22 Jul 2022 19:45:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/No-Flash-configured/m-p/1494208#M49674</guid>
      <dc:creator>bamdadslr</dc:creator>
      <dc:date>2022-07-22T19:45:11Z</dc:date>
    </item>
    <item>
      <title>Re: No Flash configured</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/No-Flash-configured/m-p/1494686#M49683</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;So do you want to download image to internal&amp;nbsp; flash or external flash?&lt;/P&gt;
&lt;P&gt;And how about first test a simple project to confirm the hardware is no problem.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Mon, 25 Jul 2022 09:11:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/No-Flash-configured/m-p/1494686#M49683</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2022-07-25T09:11:31Z</dc:date>
    </item>
    <item>
      <title>Re: No Flash configured</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/No-Flash-configured/m-p/1494863#M49686</link>
      <description>&lt;P&gt;Hi Alice_Yang,&lt;/P&gt;&lt;P&gt;Thank you for your response. I want to download it to the external flash. From the console message that I attached to my first message, it seems that the internal flash could be successfully programmed, but not the external one. Is there any sample project for LPC4088 that I can try to verify the hardware is working and see how to manage it?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Mon, 25 Jul 2022 13:53:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/No-Flash-configured/m-p/1494863#M49686</guid>
      <dc:creator>bamdadslr</dc:creator>
      <dc:date>2022-07-25T13:53:14Z</dc:date>
    </item>
    <item>
      <title>Re: No Flash configured</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/No-Flash-configured/m-p/1496291#M49702</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;From your screenshot, it seems you use both internal and external flash, I don't think the IDE can download both flash at the same time. How about create a project only use external flash, and use&amp;nbsp; flash driver "LPC40xx_SPIFI_GENERIC.cfx" do download, also delete the internal flash:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Alice_Yang_0-1658914425560.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/188042iEAD4DD71BFDAE2C5/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Alice_Yang_0-1658914425560.png" alt="Alice_Yang_0-1658914425560.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;There is demo under LPCopen, while they all use internal flash, you can change base on them.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Jul 2022 09:34:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/No-Flash-configured/m-p/1496291#M49702</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2022-07-27T09:34:29Z</dc:date>
    </item>
  </channel>
</rss>