<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 UART</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/UART/m-p/1494291#M49675</link>
    <description>&lt;PRE&gt;&lt;SPAN class=""&gt;USE MICRO LPC546XX I WANT TO ACTIVATE THE UART IN MULTIDROP MODE (9 BIT). WHEN I HAVE TO SEND 8 BYTES HOW DO I RETURN THE FIRST BYTE ADDRESS (BIT 9 = 1) AND THE REMAINING 7 BYTEES AS DATA WITH (BIT9 = 0)&lt;/SPAN&gt;&lt;/PRE&gt;</description>
    <pubDate>Sat, 23 Jul 2022 07:32:04 GMT</pubDate>
    <dc:creator>Sebastiano65</dc:creator>
    <dc:date>2022-07-23T07:32:04Z</dc:date>
    <item>
      <title>UART</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/UART/m-p/1494291#M49675</link>
      <description>&lt;PRE&gt;&lt;SPAN class=""&gt;USE MICRO LPC546XX I WANT TO ACTIVATE THE UART IN MULTIDROP MODE (9 BIT). WHEN I HAVE TO SEND 8 BYTES HOW DO I RETURN THE FIRST BYTE ADDRESS (BIT 9 = 1) AND THE REMAINING 7 BYTEES AS DATA WITH (BIT9 = 0)&lt;/SPAN&gt;&lt;/PRE&gt;</description>
      <pubDate>Sat, 23 Jul 2022 07:32:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/UART/m-p/1494291#M49675</guid>
      <dc:creator>Sebastiano65</dc:creator>
      <dc:date>2022-07-23T07:32:04Z</dc:date>
    </item>
    <item>
      <title>Re: UART</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/UART/m-p/1495361#M49690</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;How about refer to UART demos under SDK:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Alice_Yang_0-1658821158508.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/187824iBA9E7F265726C12A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Alice_Yang_0-1658821158508.png" alt="Alice_Yang_0-1658821158508.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 26 Jul 2022 07:39:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/UART/m-p/1495361#M49690</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2022-07-26T07:39:27Z</dc:date>
    </item>
  </channel>
</rss>