<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC3131 DFU mode not working in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC3131-DFU-mode-not-working/m-p/1491656#M49638</link>
    <description>&lt;P&gt;After set GP0-3, the devce enter DFU mode(got a usb device, vid/pid = 0471/df55)&lt;/P&gt;&lt;P&gt;With 'dfu-util -D /path/to/rom' command, it works fine but not as expected.&lt;/P&gt;&lt;P&gt;As states in user manual Fig18 USB DFU boot mode, if a valid image it received, it will disconnect USB and run the code(no toggle is observed on GPIO2, so I assume it is valid).&lt;/P&gt;&lt;P&gt;But my code seems not running.&lt;/P&gt;&lt;P&gt;With argument -R for dfu-util still not working, and output shows it can't detach(The Device Firmware Update Functioal Descriptor shows CanDowload only in bmAttribute, so it is as expected)&lt;/P&gt;&lt;P&gt;With arguement -a 0 or 1 for dfu-util also not working, and I do not understand the meaning(&lt;A href="http://dfu-util.sourceforge.net/dfu-util.1.html" target="_blank"&gt;DFU-UTIL (sourceforge.net)&lt;/A&gt;)&lt;/P&gt;&lt;P&gt;The code is generated with 'lpc313xImgCreator -pd' which has no prblem&lt;/P&gt;&lt;P&gt;How can I program flash or run code directly on RAM in DFU mode?&lt;/P&gt;</description>
    <pubDate>Tue, 19 Jul 2022 09:16:43 GMT</pubDate>
    <dc:creator>KM_1688</dc:creator>
    <dc:date>2022-07-19T09:16:43Z</dc:date>
    <item>
      <title>LPC3131 DFU mode not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC3131-DFU-mode-not-working/m-p/1491656#M49638</link>
      <description>&lt;P&gt;After set GP0-3, the devce enter DFU mode(got a usb device, vid/pid = 0471/df55)&lt;/P&gt;&lt;P&gt;With 'dfu-util -D /path/to/rom' command, it works fine but not as expected.&lt;/P&gt;&lt;P&gt;As states in user manual Fig18 USB DFU boot mode, if a valid image it received, it will disconnect USB and run the code(no toggle is observed on GPIO2, so I assume it is valid).&lt;/P&gt;&lt;P&gt;But my code seems not running.&lt;/P&gt;&lt;P&gt;With argument -R for dfu-util still not working, and output shows it can't detach(The Device Firmware Update Functioal Descriptor shows CanDowload only in bmAttribute, so it is as expected)&lt;/P&gt;&lt;P&gt;With arguement -a 0 or 1 for dfu-util also not working, and I do not understand the meaning(&lt;A href="http://dfu-util.sourceforge.net/dfu-util.1.html" target="_blank"&gt;DFU-UTIL (sourceforge.net)&lt;/A&gt;)&lt;/P&gt;&lt;P&gt;The code is generated with 'lpc313xImgCreator -pd' which has no prblem&lt;/P&gt;&lt;P&gt;How can I program flash or run code directly on RAM in DFU mode?&lt;/P&gt;</description>
      <pubDate>Tue, 19 Jul 2022 09:16:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC3131-DFU-mode-not-working/m-p/1491656#M49638</guid>
      <dc:creator>KM_1688</dc:creator>
      <dc:date>2022-07-19T09:16:43Z</dc:date>
    </item>
    <item>
      <title>Re: LPC3131 DFU mode not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC3131-DFU-mode-not-working/m-p/1496293#M49703</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Have you test your image without DFU mode, just download it with normal mode, does it can work well?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Wed, 27 Jul 2022 09:40:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC3131-DFU-mode-not-working/m-p/1496293#M49703</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2022-07-27T09:40:08Z</dc:date>
    </item>
    <item>
      <title>Re: LPC3131 DFU mode not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC3131-DFU-mode-not-working/m-p/1496804#M49711</link>
      <description>&lt;P&gt;Yes, work with normal mode.&lt;/P&gt;</description>
      <pubDate>Thu, 28 Jul 2022 01:09:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC3131-DFU-mode-not-working/m-p/1496804#M49711</guid>
      <dc:creator>KM_1688</dc:creator>
      <dc:date>2022-07-28T01:09:48Z</dc:date>
    </item>
    <item>
      <title>Re: LPC3131 DFU mode not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC3131-DFU-mode-not-working/m-p/1499869#M49748</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Can you read the flash, compare value with your image.&lt;/P&gt;</description>
      <pubDate>Wed, 03 Aug 2022 01:24:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC3131-DFU-mode-not-working/m-p/1499869#M49748</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2022-08-03T01:24:28Z</dc:date>
    </item>
  </channel>
</rss>