<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 LPC546xx with 1.8V design and USB</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-with-1-8V-design-and-USB/m-p/1489546#M49611</link>
    <description>&lt;P&gt;I want to start a LPC546xx design with 1.8V - how can i use USB0?&lt;/P&gt;</description>
    <pubDate>Thu, 14 Jul 2022 14:11:26 GMT</pubDate>
    <dc:creator>RU</dc:creator>
    <dc:date>2022-07-14T14:11:26Z</dc:date>
    <item>
      <title>LPC546xx with 1.8V design and USB</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-with-1-8V-design-and-USB/m-p/1489546#M49611</link>
      <description>&lt;P&gt;I want to start a LPC546xx design with 1.8V - how can i use USB0?&lt;/P&gt;</description>
      <pubDate>Thu, 14 Jul 2022 14:11:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-with-1-8V-design-and-USB/m-p/1489546#M49611</guid>
      <dc:creator>RU</dc:creator>
      <dc:date>2022-07-14T14:11:26Z</dc:date>
    </item>
    <item>
      <title>Re: LPC546xx with 1.8V design and USB</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-with-1-8V-design-and-USB/m-p/1489953#M49619</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;First of all, pls download the data sheet of LPC546xx from the link:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com.cn/docs/en/data-sheet/LPC546XX.pdf" target="_blank"&gt;https://www.nxp.com.cn/docs/en/data-sheet/LPC546XX.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;As the following screenshot from above data sheet, you can see that&lt;/P&gt;
&lt;P&gt;typical voltage of USB1_AVDD3V3,USB1_AVDDTX3V3 pins are 3.3V&lt;/P&gt;
&lt;P&gt;The VDD is from 1.71 to 3.6V, but if you use USB, you have to meet the following condition:&lt;/P&gt;
&lt;P&gt;For USB full-speed operation only 3.0 - 3.6 V&lt;BR /&gt;For USB high-speed operation only 1.71 - 3.6 V&lt;/P&gt;
&lt;P&gt;the VDDA is from 1.71 to 3.6V.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1657851775481.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/186722iE21FED803D1B4198/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1657851775481.png" alt="xiangjun_rong_0-1657851775481.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 15 Jul 2022 02:27:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-with-1-8V-design-and-USB/m-p/1489953#M49619</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-07-15T02:27:10Z</dc:date>
    </item>
    <item>
      <title>Re: LPC546xx with 1.8V design and USB</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-with-1-8V-design-and-USB/m-p/1501788#M49777</link>
      <description>&lt;P&gt;Table 12 says for VDD 1.71V .. 3.6V for USB high speed only.&amp;nbsp;According to this, USB would work with 1.8V.&lt;/P&gt;&lt;P&gt;On the other hand, table 21 shows quite contradictory values. Is USB now possible with 1.8V?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="RU_0-1659700050452.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/189266iF09D22FEAF381EEA/image-size/medium?v=v2&amp;amp;px=400" role="button" title="RU_0-1659700050452.png" alt="RU_0-1659700050452.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 05 Aug 2022 11:48:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-with-1-8V-design-and-USB/m-p/1501788#M49777</guid>
      <dc:creator>RU</dc:creator>
      <dc:date>2022-08-05T11:48:26Z</dc:date>
    </item>
    <item>
      <title>Re: LPC546xx with 1.8V design and USB</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-with-1-8V-design-and-USB/m-p/1505513#M49833</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I think it is correct:&lt;/P&gt;
&lt;P&gt;The VDD is from 1.71 to 3.6V, but if you use USB, you have to meet the following condition:&lt;/P&gt;
&lt;P&gt;For USB full-speed operation only 3.0 - 3.6 V&lt;BR /&gt;For USB high-speed operation only 1.71 - 3.6 V&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Fri, 12 Aug 2022 09:25:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-with-1-8V-design-and-USB/m-p/1505513#M49833</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-08-12T09:25:30Z</dc:date>
    </item>
  </channel>
</rss>