<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic ISP on LPC55S28 using SPI on Flexcomm 3 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/ISP-on-LPC55S28-using-SPI-on-Flexcomm-3/m-p/1488304#M49572</link>
    <description>&lt;P&gt;We'd planned on using SPI on Flexcomm 3 for ISP but I've found a footnote in UM11126 -&amp;nbsp;LPC55S6x/LPC55S2x/LPC552x User manual in Table 176 on page 141 that says "SPI ISP mode on Flexcomm 3 is supported on device revision A0 only."&amp;nbsp; I haven't been able corroborate that statement with another document.&amp;nbsp; Other documents suggest that ISP can be performed on either Flexcomm 3 or SPI_HS.&amp;nbsp; It would be really advantageous if we could implement the SPI on Flexcomm 3.&amp;nbsp; Can someone corroborate or contradict the assertion that SPI on Flexcomm 3 cannot be used on devices with revision newer than A0?&lt;/P&gt;</description>
    <pubDate>Tue, 12 Jul 2022 19:28:13 GMT</pubDate>
    <dc:creator>WilliamW</dc:creator>
    <dc:date>2022-07-12T19:28:13Z</dc:date>
    <item>
      <title>ISP on LPC55S28 using SPI on Flexcomm 3</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ISP-on-LPC55S28-using-SPI-on-Flexcomm-3/m-p/1488304#M49572</link>
      <description>&lt;P&gt;We'd planned on using SPI on Flexcomm 3 for ISP but I've found a footnote in UM11126 -&amp;nbsp;LPC55S6x/LPC55S2x/LPC552x User manual in Table 176 on page 141 that says "SPI ISP mode on Flexcomm 3 is supported on device revision A0 only."&amp;nbsp; I haven't been able corroborate that statement with another document.&amp;nbsp; Other documents suggest that ISP can be performed on either Flexcomm 3 or SPI_HS.&amp;nbsp; It would be really advantageous if we could implement the SPI on Flexcomm 3.&amp;nbsp; Can someone corroborate or contradict the assertion that SPI on Flexcomm 3 cannot be used on devices with revision newer than A0?&lt;/P&gt;</description>
      <pubDate>Tue, 12 Jul 2022 19:28:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ISP-on-LPC55S28-using-SPI-on-Flexcomm-3/m-p/1488304#M49572</guid>
      <dc:creator>WilliamW</dc:creator>
      <dc:date>2022-07-12T19:28:13Z</dc:date>
    </item>
    <item>
      <title>Re: ISP on LPC55S28 using SPI on Flexcomm 3</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ISP-on-LPC55S28-using-SPI-on-Flexcomm-3/m-p/1488367#M49574</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/9160"&gt;@WilliamW&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;I'm afraid the RM is correct.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;For revision A0 of the LPC55S69, two SPI modules are supported in ISP mode: FC3 and HS_SPI.&lt;BR /&gt;&lt;/SPAN&gt;However, for revision 1B, only HS_SPI supports it.&lt;BR /&gt;&lt;BR /&gt;This is also the case for the LPC55S28.&lt;BR /&gt;&lt;BR /&gt;BR,&lt;/P&gt;
&lt;P&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Wed, 13 Jul 2022 00:28:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ISP-on-LPC55S28-using-SPI-on-Flexcomm-3/m-p/1488367#M49574</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2022-07-13T00:28:57Z</dc:date>
    </item>
  </channel>
</rss>