<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Problem Programming LPC804 Xpresso Board using windows 11</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-Programming-LPC804-Xpresso-Board-using-windows-11/m-p/1482937#M49400</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using McuXpresso on a windows 11 machine and I am trying to program the LPCXpresso804 board's MCU. The Probe is detected, but then an error indicates that the Probe is not open.&lt;/P&gt;&lt;P&gt;I have installed the windows USB driver for LPC probe LPC11Uxx_Debug_Probe_VCOM_v1.0.0.EXE, which indicates version 1.0.7 (Jully 2018) in its readme file.&lt;/P&gt;&lt;P&gt;The very same board with same cable can be easily programmed when using McuXpresso on a Ubuntu 20.04 machine, so the board is OK.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does anyone is using a LPC Probe form windows 11 ? Is this a driver issue?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Milix&lt;/P&gt;</description>
    <pubDate>Thu, 30 Jun 2022 16:33:56 GMT</pubDate>
    <dc:creator>Milix</dc:creator>
    <dc:date>2022-06-30T16:33:56Z</dc:date>
    <item>
      <title>Problem Programming LPC804 Xpresso Board using windows 11</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-Programming-LPC804-Xpresso-Board-using-windows-11/m-p/1482937#M49400</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using McuXpresso on a windows 11 machine and I am trying to program the LPCXpresso804 board's MCU. The Probe is detected, but then an error indicates that the Probe is not open.&lt;/P&gt;&lt;P&gt;I have installed the windows USB driver for LPC probe LPC11Uxx_Debug_Probe_VCOM_v1.0.0.EXE, which indicates version 1.0.7 (Jully 2018) in its readme file.&lt;/P&gt;&lt;P&gt;The very same board with same cable can be easily programmed when using McuXpresso on a Ubuntu 20.04 machine, so the board is OK.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does anyone is using a LPC Probe form windows 11 ? Is this a driver issue?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Milix&lt;/P&gt;</description>
      <pubDate>Thu, 30 Jun 2022 16:33:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-Programming-LPC804-Xpresso-Board-using-windows-11/m-p/1482937#M49400</guid>
      <dc:creator>Milix</dc:creator>
      <dc:date>2022-06-30T16:33:56Z</dc:date>
    </item>
    <item>
      <title>Re: Problem Programming LPC804 Xpresso Board using windows 11</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-Programming-LPC804-Xpresso-Board-using-windows-11/m-p/1483974#M49443</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;How about pressing ISP pin all the time when connecting?&lt;BR /&gt;If still have issue, please take a video or screenshot to show your steps.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Mon, 04 Jul 2022 09:32:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-Programming-LPC804-Xpresso-Board-using-windows-11/m-p/1483974#M49443</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2022-07-04T09:32:31Z</dc:date>
    </item>
  </channel>
</rss>