<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: OM13054 (LPC-Link 2) Board is not working</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/OM13054-LPC-Link-2-Board-is-not-working/m-p/1480954#M49353</link>
    <description>&lt;P&gt;Thank you sir. Now problem is solved!&lt;/P&gt;</description>
    <pubDate>Tue, 28 Jun 2022 06:17:39 GMT</pubDate>
    <dc:creator>dhjeong</dc:creator>
    <dc:date>2022-06-28T06:17:39Z</dc:date>
    <item>
      <title>OM13054 (LPC-Link 2) Board is not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/OM13054-LPC-Link-2-Board-is-not-working/m-p/1477935#M49276</link>
      <description>&lt;PRE&gt;&lt;SPAN class=""&gt;hello. I am using an OM13054 (LPC-Link 2) board and flashing the firmware using the ARM 20-10 JTAG Connector.

The firmware flash tool uses the built-in Flash tool in MCUXpresso IDE :)

However, when I run debug for testing, I get an unexpected error.&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The OM13054 (lpc-link-2) board is connected to the PC via micro USB.&lt;/SPAN&gt;

Here are the errors:&lt;BR /&gt;&lt;/SPAN&gt;&lt;/PRE&gt;&lt;P&gt;Unable to connect wire for probe index 1.&lt;BR /&gt;Error: Wire Ack Fault - target connected?&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;For more information about the error, I have attached a photo. Please check the attached file.&lt;/SPAN&gt;&lt;/P&gt;&lt;PRE&gt;&lt;SPAN class=""&gt;Do you have any guides on how to solve this problem??&lt;/SPAN&gt;&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 22 Jun 2022 07:43:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/OM13054-LPC-Link-2-Board-is-not-working/m-p/1477935#M49276</guid>
      <dc:creator>dhjeong</dc:creator>
      <dc:date>2022-06-22T07:43:59Z</dc:date>
    </item>
    <item>
      <title>Re: OM13054 (LPC-Link 2) Board is not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/OM13054-LPC-Link-2-Board-is-not-working/m-p/1478199#M49280</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;When you use LPC-Link2 debug a target, Could you please check in windows manager if LPC-Link2 is correctly recognized?&lt;/P&gt;
&lt;P&gt;Not sure if on board LPC-Link2 firmware is damaged, Please try to update LPC-Link2 firmware with LPCScrypt for either CMSIS-DAP and Jlink . can it update successfully? ( Note, all ensure that jumper JP1 is NOT fitted so that the probe will be DFU bootable at power on. after the firmware update, remove JP1, power off and power on)&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/microcontrollers-developer-resources/lpcscrypt-v2-1-2:LPCSCRYPT" target="_blank"&gt;https://www.nxp.com/design/microcontrollers-developer-resources/lpcscrypt-v2-1-2:LPCSCRYPT&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 22 Jun 2022 12:50:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/OM13054-LPC-Link-2-Board-is-not-working/m-p/1478199#M49280</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2022-06-22T12:50:25Z</dc:date>
    </item>
    <item>
      <title>Re: OM13054 (LPC-Link 2) Board is not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/OM13054-LPC-Link-2-Board-is-not-working/m-p/1478551#M49284</link>
      <description>&lt;P&gt;thank you i'm also trying on Mac OS Montrey, but I get Read timeout error on Mac OS. Can you tell me what the problem is?&lt;/P&gt;&lt;P&gt;attach the photo.&lt;/P&gt;</description>
      <pubDate>Thu, 23 Jun 2022 00:18:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/OM13054-LPC-Link-2-Board-is-not-working/m-p/1478551#M49284</guid>
      <dc:creator>dhjeong</dc:creator>
      <dc:date>2022-06-23T00:18:49Z</dc:date>
    </item>
    <item>
      <title>Re: OM13054 (LPC-Link 2) Board is not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/OM13054-LPC-Link-2-Board-is-not-working/m-p/1478558#M49285</link>
      <description>&lt;P&gt;Do I need to supply power to the JP1 pin for LPC-LINK2 firmware update?&lt;/P&gt;&lt;P&gt;Although connected to PC via USB port, "Nothing to boot" is console output.&lt;/P&gt;</description>
      <pubDate>Thu, 23 Jun 2022 00:44:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/OM13054-LPC-Link-2-Board-is-not-working/m-p/1478558#M49285</guid>
      <dc:creator>dhjeong</dc:creator>
      <dc:date>2022-06-23T00:44:01Z</dc:date>
    </item>
    <item>
      <title>Re: OM13054 (LPC-Link 2) Board is not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/OM13054-LPC-Link-2-Board-is-not-working/m-p/1478623#M49287</link>
      <description>&lt;P&gt;The equipment for LPC-Link2 is recognized normally. (USB port to PC)&lt;/P&gt;</description>
      <pubDate>Thu, 23 Jun 2022 02:12:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/OM13054-LPC-Link-2-Board-is-not-working/m-p/1478623#M49287</guid>
      <dc:creator>dhjeong</dc:creator>
      <dc:date>2022-06-23T02:12:44Z</dc:date>
    </item>
    <item>
      <title>Re: OM13054 (LPC-Link 2) Board is not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/OM13054-LPC-Link-2-Board-is-not-working/m-p/1479219#M49303</link>
      <description>&lt;P&gt;To update LPC-Link2 with LPCscrypt&lt;/P&gt;
&lt;OL&gt;
&lt;LI&gt;Install LPCScrypt&lt;/LI&gt;
&lt;LI&gt;For LPC-Link2: remove link JP1 (nearest USB), for LPCXpresso V2/V3: make DFU link&lt;/LI&gt;
&lt;LI&gt;Connect the probe to the host via USB&lt;/LI&gt;
&lt;LI&gt;Run the desired programming script (CMSIS or Jlink)&lt;/LI&gt;
&lt;LI&gt;For LPC-Link2: restore link JP1 (nearest USB), for LPCXpresso V2/V3: remove DFU link&lt;/LI&gt;
&lt;LI&gt;Re-power the board and try debug code with IDE&lt;/LI&gt;
&lt;/OL&gt;
&lt;P&gt;If CMSIS-DAP interface can't be connect with IDE, try Jlink interface,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Thu, 23 Jun 2022 15:45:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/OM13054-LPC-Link-2-Board-is-not-working/m-p/1479219#M49303</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2022-06-23T15:45:45Z</dc:date>
    </item>
    <item>
      <title>Re: OM13054 (LPC-Link 2) Board is not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/OM13054-LPC-Link-2-Board-is-not-working/m-p/1480954#M49353</link>
      <description>&lt;P&gt;Thank you sir. Now problem is solved!&lt;/P&gt;</description>
      <pubDate>Tue, 28 Jun 2022 06:17:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/OM13054-LPC-Link-2-Board-is-not-working/m-p/1480954#M49353</guid>
      <dc:creator>dhjeong</dc:creator>
      <dc:date>2022-06-28T06:17:39Z</dc:date>
    </item>
  </channel>
</rss>