<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IBIS Model Acronym Definitions in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/IBIS-Model-Acronym-Definitions/m-p/1476009#M49231</link>
    <description>&lt;P&gt;I was able to confirm some of my questions using the IBIS Modeling Cookbook.&amp;nbsp; In it, it states that each model can be for Input, Output, or I/O, so that is clear to me now. It is also clear that the PU model is to be used for output driving high, and the PD model is to be used for output driving low.&amp;nbsp; What remains unclear is the following:&lt;BR /&gt;&lt;BR /&gt;RP means ?&lt;/P&gt;&lt;P&gt;ZS means?&lt;/P&gt;&lt;P&gt;HS means?&lt;/P&gt;&lt;P&gt;LS means?&lt;/P&gt;</description>
    <pubDate>Fri, 17 Jun 2022 12:16:07 GMT</pubDate>
    <dc:creator>wleismer</dc:creator>
    <dc:date>2022-06-17T12:16:07Z</dc:date>
    <item>
      <title>IBIS Model Acronym Definitions</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/IBIS-Model-Acronym-Definitions/m-p/1475545#M49214</link>
      <description>&lt;P&gt;Hello, I am working with the LPC54Sxx IBIS model, and it is unclear to me which models are intended to be used to confirm signal integrity as a pin outputs to a transmission line.&amp;nbsp; For example, there are two main models, MFIOHST5V_3V3_XX_ZZ and&amp;nbsp;MFIOT5V_3V3_XX_ZZ&lt;/P&gt;&lt;P&gt;Where: XX can be PU,PD,RP,ZS and ZZ can be HS or LS.&lt;/P&gt;&lt;P&gt;I understand that PU = Pull Up, PD = Pull Down, but what does RP = ? and ZS = ? (I'm guessing high impedance?).&amp;nbsp; Is HS = High Speed and LS = Low Speed?&lt;/P&gt;&lt;P&gt;If I want to model the effects on signal integrity from PIO0_16 (ball M4 on the 180 pin BGA), which is Ethernet TXD_0 Out, which model should I use?&lt;/P&gt;&lt;P&gt;Here is the LPC54Sxx page, where the datasheet and IBIS model are located: &lt;A href="https://www.nxp.com/part/LPC54S016JBD100#/" target="_blank"&gt;https://www.nxp.com/part/LPC54S016JBD100#/&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 16 Jun 2022 21:01:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/IBIS-Model-Acronym-Definitions/m-p/1475545#M49214</guid>
      <dc:creator>wleismer</dc:creator>
      <dc:date>2022-06-16T21:01:09Z</dc:date>
    </item>
    <item>
      <title>Re: IBIS Model Acronym Definitions</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/IBIS-Model-Acronym-Definitions/m-p/1476009#M49231</link>
      <description>&lt;P&gt;I was able to confirm some of my questions using the IBIS Modeling Cookbook.&amp;nbsp; In it, it states that each model can be for Input, Output, or I/O, so that is clear to me now. It is also clear that the PU model is to be used for output driving high, and the PD model is to be used for output driving low.&amp;nbsp; What remains unclear is the following:&lt;BR /&gt;&lt;BR /&gt;RP means ?&lt;/P&gt;&lt;P&gt;ZS means?&lt;/P&gt;&lt;P&gt;HS means?&lt;/P&gt;&lt;P&gt;LS means?&lt;/P&gt;</description>
      <pubDate>Fri, 17 Jun 2022 12:16:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/IBIS-Model-Acronym-Definitions/m-p/1476009#M49231</guid>
      <dc:creator>wleismer</dc:creator>
      <dc:date>2022-06-17T12:16:07Z</dc:date>
    </item>
    <item>
      <title>Re: IBIS Model Acronym Definitions</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/IBIS-Model-Acronym-Definitions/m-p/1476395#M49234</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;A id="link_6" class="lia-link-navigation lia-page-link lia-user-name-link" href="https://community.nxp.com/t5/user/viewprofilepage/user-id/202383" target="_self" aria-label="View Profile of wleismer"&gt;&lt;SPAN class=""&gt;wleismer&lt;/SPAN&gt;&lt;/A&gt;,&lt;/P&gt;
&lt;P&gt;I will help to confirm with design team. then tell you .ASAP.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Mon, 20 Jun 2022 02:37:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/IBIS-Model-Acronym-Definitions/m-p/1476395#M49234</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2022-06-20T02:37:12Z</dc:date>
    </item>
    <item>
      <title>Re: IBIS Model Acronym Definitions</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/IBIS-Model-Acronym-Definitions/m-p/1476828#M49255</link>
      <description>&lt;P&gt;Thanks Alice!&lt;/P&gt;</description>
      <pubDate>Mon, 20 Jun 2022 13:00:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/IBIS-Model-Acronym-Definitions/m-p/1476828#M49255</guid>
      <dc:creator>wleismer</dc:creator>
      <dc:date>2022-06-20T13:00:52Z</dc:date>
    </item>
    <item>
      <title>Re: IBIS Model Acronym Definitions</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/IBIS-Model-Acronym-Definitions/m-p/1482291#M49378</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/202383" target="_self"&gt;&lt;SPAN class=""&gt;wleismer,&lt;/SPAN&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt; The definitions are below and can be controlled via IOCON register.&lt;/P&gt;&lt;P&gt;Hs – slew rate is fast mode&lt;/P&gt;&lt;P&gt;Ls – slew rate is standard mode&lt;/P&gt;&lt;P&gt;Rp – simulated open drain mode enabled&lt;/P&gt;&lt;P&gt;PU means internal pull-up enabled&lt;/P&gt;&lt;P&gt;PD means internal pull-down enabled&lt;/P&gt;&lt;P&gt;ZS – disable internal pull-up and disable internal pull-down&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Use the MFIOT5V model since pad type for PIO0_16 is MFIOT5V&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Thu, 30 Jun 2022 01:56:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/IBIS-Model-Acronym-Definitions/m-p/1482291#M49378</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2022-06-30T01:56:49Z</dc:date>
    </item>
    <item>
      <title>Re: IBIS Model Acronym Definitions</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/IBIS-Model-Acronym-Definitions/m-p/1482825#M49398</link>
      <description>&lt;P&gt;Excellent, thank you so much Alice!&lt;/P&gt;</description>
      <pubDate>Thu, 30 Jun 2022 14:17:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/IBIS-Model-Acronym-Definitions/m-p/1482825#M49398</guid>
      <dc:creator>wleismer</dc:creator>
      <dc:date>2022-06-30T14:17:01Z</dc:date>
    </item>
    <item>
      <title>Re: IBIS Model Acronym Definitions</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/IBIS-Model-Acronym-Definitions/m-p/1483952#M49440</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;A id="link_6" class="lia-link-navigation lia-page-link lia-user-name-link" href="https://community.nxp.com/t5/user/viewprofilepage/user-id/202383" target="_self" aria-label="View Profile of wleismer"&gt;&lt;SPAN class=""&gt;wleismer&lt;/SPAN&gt;&lt;/A&gt;,&lt;/P&gt;
&lt;P&gt;Welcome!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Mon, 04 Jul 2022 09:10:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/IBIS-Model-Acronym-Definitions/m-p/1483952#M49440</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2022-07-04T09:10:13Z</dc:date>
    </item>
  </channel>
</rss>