<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: LPC546xx: USB1_REXT when USB1 is unused</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-USB1-REXT-when-USB1-is-unused/m-p/1473747#M49158</link>
    <description>&lt;BLOCKQUOTE&gt;&lt;P&gt;&lt;SPAN&gt;You can leave the UBS1_REXT pin unconnected if you are not using USB1 functions. And if you have connected the USB1_VBUS, USB1_AVDDC3V3, USB1_AVDDTX3V3 and USB1_AVSSTX3V3 to VDD it doesn’t affect the UDB1_DM, USB1_DP and USB1_REXT.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;SPAN&gt;Ok, thank you for the answer. However I think you made an error with&amp;nbsp;USB1_AVSSTX3V3: this pin should be tied to VSS, not VDD.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 14 Jun 2022 15:13:20 GMT</pubDate>
    <dc:creator>giusloq</dc:creator>
    <dc:date>2022-06-14T15:13:20Z</dc:date>
    <item>
      <title>LPC546xx: USB1_REXT when USB1 is unused</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-USB1-REXT-when-USB1-is-unused/m-p/1472220#M49132</link>
      <description>&lt;P&gt;Should I connect USB1_REXT pin to an external resistor even when USB1 is not used on the board? What happens if UDB1_DM/USB1_DP/USB1_REXT are not connected, while USB1 VDD signals (USB1_AVDDC3V3, USB1_AVDDTX3V3, USB1_VBUS) are tied to VDD?&lt;/P&gt;&lt;P&gt;I found recommended connections of some unused pins in the datasheet, but USB1_REXT is not descripted.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 10 Jun 2022 11:40:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-USB1-REXT-when-USB1-is-unused/m-p/1472220#M49132</guid>
      <dc:creator>giusloq</dc:creator>
      <dc:date>2022-06-10T11:40:50Z</dc:date>
    </item>
    <item>
      <title>Re: LPC546xx: USB1_REXT when USB1 is unused</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-USB1-REXT-when-USB1-is-unused/m-p/1473041#M49146</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160419"&gt;@giusloq&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can leave the UBS1_REXT pin unconnected if you are not using USB1 functions. And if you have connected the USB1_VBUS, USB1_AVDDC3V3 and USB1_AVDDTX3V3 to VDD it doesn’t affect the UDB1_DM, USB1_DP and USB1_REXT.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;B.R.&lt;/P&gt;
&lt;P&gt;VaneB&lt;/P&gt;</description>
      <pubDate>Tue, 14 Jun 2022 15:43:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-USB1-REXT-when-USB1-is-unused/m-p/1473041#M49146</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2022-06-14T15:43:49Z</dc:date>
    </item>
    <item>
      <title>Re: LPC546xx: USB1_REXT when USB1 is unused</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-USB1-REXT-when-USB1-is-unused/m-p/1473747#M49158</link>
      <description>&lt;BLOCKQUOTE&gt;&lt;P&gt;&lt;SPAN&gt;You can leave the UBS1_REXT pin unconnected if you are not using USB1 functions. And if you have connected the USB1_VBUS, USB1_AVDDC3V3, USB1_AVDDTX3V3 and USB1_AVSSTX3V3 to VDD it doesn’t affect the UDB1_DM, USB1_DP and USB1_REXT.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;SPAN&gt;Ok, thank you for the answer. However I think you made an error with&amp;nbsp;USB1_AVSSTX3V3: this pin should be tied to VSS, not VDD.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 14 Jun 2022 15:13:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-USB1-REXT-when-USB1-is-unused/m-p/1473747#M49158</guid>
      <dc:creator>giusloq</dc:creator>
      <dc:date>2022-06-14T15:13:20Z</dc:date>
    </item>
  </channel>
</rss>