<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Power supply pins in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Power-supply-pins/m-p/514037#M490</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by IanB on Fri Jan 02 06:00:54 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm just about to use the LPC1518 in the 100-pin package, which has six of each Vdd and Vss pins.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;How many of these need to be connected for the device to work properly?&amp;nbsp; Connecting all the Vdd pins together is the only thing that is preventing me from getting the project on a single-sided pcb!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Having checked an LPC1111 with a continuity tester, I know that its two Vdd pins are not internally connected, and I found out the hard way that they both have to be connected for it to work properly. Is it the same with the 100-pin TQFP? I couldn't find much information in either the data sheet or the user manual, just that the "absolute maximum" rating for the supply current is 100mA per supply pin.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If the supply pins are not internally connected, then how would I calculate how much current goes down each pin?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:09:51 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:09:51Z</dc:date>
    <item>
      <title>Power supply pins</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Power-supply-pins/m-p/514037#M490</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by IanB on Fri Jan 02 06:00:54 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm just about to use the LPC1518 in the 100-pin package, which has six of each Vdd and Vss pins.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;How many of these need to be connected for the device to work properly?&amp;nbsp; Connecting all the Vdd pins together is the only thing that is preventing me from getting the project on a single-sided pcb!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Having checked an LPC1111 with a continuity tester, I know that its two Vdd pins are not internally connected, and I found out the hard way that they both have to be connected for it to work properly. Is it the same with the 100-pin TQFP? I couldn't find much information in either the data sheet or the user manual, just that the "absolute maximum" rating for the supply current is 100mA per supply pin.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If the supply pins are not internally connected, then how would I calculate how much current goes down each pin?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:09:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Power-supply-pins/m-p/514037#M490</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:09:51Z</dc:date>
    </item>
    <item>
      <title>Re: Power supply pins</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Power-supply-pins/m-p/514038#M491</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by starblue on Mon Jan 05 10:12:16 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;My understanding is that you should always connect all Vdd/Vss pins, and use a decoupling cap close to each pair.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:09:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Power-supply-pins/m-p/514038#M491</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:09:52Z</dc:date>
    </item>
    <item>
      <title>Re: Power supply pins</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Power-supply-pins/m-p/514039#M492</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by nerd herd on Mon Jan 05 11:43:41 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi IanB,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In order to ensure correct operation, it is recommended to connect all the Vdd pins to the digital 3.3V rail with a decoupling capacitor like Starblue stated.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:09:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Power-supply-pins/m-p/514039#M492</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:09:53Z</dc:date>
    </item>
    <item>
      <title>Re: Power supply pins</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Power-supply-pins/m-p/514040#M493</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by IanB on Mon Jan 05 15:20:59 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I thought so, but I was just hoping I could get away with fewer. . .&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:09:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Power-supply-pins/m-p/514040#M493</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:09:53Z</dc:date>
    </item>
  </channel>
</rss>