<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 LPC54608 SPIFI RAM</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-SPIFI-RAM/m-p/1461549#M48847</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;we wanted to use LPC54608 but we need more RAM and we can't use SDRAM(EMC), we need the other pin functions.&lt;/P&gt;&lt;P&gt;That's why we want to connect the external RAM is through SPIFI.&lt;BR /&gt;At startup the firmware configures the SPIFI to command mode. Copies the data from the USB or SPI to the SPIFI Ram and executes it from there.&lt;/P&gt;&lt;P&gt;Are there any problems with this configuration?&lt;/P&gt;</description>
    <pubDate>Fri, 20 May 2022 10:14:07 GMT</pubDate>
    <dc:creator>A_M</dc:creator>
    <dc:date>2022-05-20T10:14:07Z</dc:date>
    <item>
      <title>LPC54608 SPIFI RAM</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-SPIFI-RAM/m-p/1461549#M48847</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;we wanted to use LPC54608 but we need more RAM and we can't use SDRAM(EMC), we need the other pin functions.&lt;/P&gt;&lt;P&gt;That's why we want to connect the external RAM is through SPIFI.&lt;BR /&gt;At startup the firmware configures the SPIFI to command mode. Copies the data from the USB or SPI to the SPIFI Ram and executes it from there.&lt;/P&gt;&lt;P&gt;Are there any problems with this configuration?&lt;/P&gt;</description>
      <pubDate>Fri, 20 May 2022 10:14:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-SPIFI-RAM/m-p/1461549#M48847</guid>
      <dc:creator>A_M</dc:creator>
      <dc:date>2022-05-20T10:14:07Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54608 SPIFI RAM</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-SPIFI-RAM/m-p/1462236#M48866</link>
      <description>&lt;P&gt;HI&lt;/P&gt;
&lt;P&gt;LPC540xx can support SPIFI boot (&amp;nbsp;Boot from QSPI NOR flash device connected to SPIFI interface. ), but LPC54608 doesn't support.&lt;/P&gt;
&lt;P&gt;The available boot source for LPC546xx is as below:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ZhangJennie_0-1653290462189.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/180582i7312E7835653032E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ZhangJennie_0-1653290462189.png" alt="ZhangJennie_0-1653290462189.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;User needs to access SPIFI device from internal Flash.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 23 May 2022 07:49:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-SPIFI-RAM/m-p/1462236#M48866</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2022-05-23T07:49:11Z</dc:date>
    </item>
  </channel>
</rss>