<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: question</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/question/m-p/1459912#M48814</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;As you know that the LPC5512 has one full-speed USB, which can function as both device and host.&lt;/P&gt;
&lt;P&gt;We provide USB stack in SDK package, you can download SDK package from the link:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-software-development-kit-sdk:MCUXpresso-SDK" target="_blank"&gt;https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-software-development-kit-sdk:MCUXpresso-SDK&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;You can select the USB class example in SDK USB example for example CDC, MSC...&lt;/P&gt;
&lt;P&gt;From hardware perspective, when the USB of LPC5512 functions as a device, when a USB cable is inserted, an USB interrupt will be fired on LPC5512 side, the host can communicate with the device and exchange the descriptor inf.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun&lt;/P&gt;</description>
    <pubDate>Wed, 18 May 2022 09:44:24 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2022-05-18T09:44:24Z</dc:date>
    <item>
      <title>question</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/question/m-p/1459806#M48809</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have microcontroller&amp;nbsp;LPC5512JBD100E on my board, I have to check if the USB cable is connected with the board, and to have feedback from the controller about that. Which software do I need to have and how to do it ?&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Milan&lt;/P&gt;</description>
      <pubDate>Wed, 18 May 2022 07:30:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/question/m-p/1459806#M48809</guid>
      <dc:creator>milan021</dc:creator>
      <dc:date>2022-05-18T07:30:41Z</dc:date>
    </item>
    <item>
      <title>Re: question</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/question/m-p/1459912#M48814</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;As you know that the LPC5512 has one full-speed USB, which can function as both device and host.&lt;/P&gt;
&lt;P&gt;We provide USB stack in SDK package, you can download SDK package from the link:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-software-development-kit-sdk:MCUXpresso-SDK" target="_blank"&gt;https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-software-development-kit-sdk:MCUXpresso-SDK&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;You can select the USB class example in SDK USB example for example CDC, MSC...&lt;/P&gt;
&lt;P&gt;From hardware perspective, when the USB of LPC5512 functions as a device, when a USB cable is inserted, an USB interrupt will be fired on LPC5512 side, the host can communicate with the device and exchange the descriptor inf.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun&lt;/P&gt;</description>
      <pubDate>Wed, 18 May 2022 09:44:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/question/m-p/1459912#M48814</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-05-18T09:44:24Z</dc:date>
    </item>
  </channel>
</rss>