<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC546xx and crystal-less USB0 operation in device mode</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-and-crystal-less-USB0-operation-in-device-mode/m-p/1459754#M48808</link>
    <description>&lt;P&gt;It seems it's possible to use USB0 full-speed peripheral in device mode with only internal oscillator (without an external crystal).&lt;/P&gt;&lt;P&gt;However Errata says there's a problem with clock adjustment when the device is connected to the host through multiple bus. The work-around is:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;Use the FRO calibration library provided in TN00032. This library allows the application to&lt;BR /&gt;have a crystal-less USB device operation in full-speed mode.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I tried to search for Technical Note TN00032, but I couldn't. Where is it?&lt;/P&gt;</description>
    <pubDate>Wed, 18 May 2022 06:36:22 GMT</pubDate>
    <dc:creator>giusloq</dc:creator>
    <dc:date>2022-05-18T06:36:22Z</dc:date>
    <item>
      <title>LPC546xx and crystal-less USB0 operation in device mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-and-crystal-less-USB0-operation-in-device-mode/m-p/1459754#M48808</link>
      <description>&lt;P&gt;It seems it's possible to use USB0 full-speed peripheral in device mode with only internal oscillator (without an external crystal).&lt;/P&gt;&lt;P&gt;However Errata says there's a problem with clock adjustment when the device is connected to the host through multiple bus. The work-around is:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;Use the FRO calibration library provided in TN00032. This library allows the application to&lt;BR /&gt;have a crystal-less USB device operation in full-speed mode.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I tried to search for Technical Note TN00032, but I couldn't. Where is it?&lt;/P&gt;</description>
      <pubDate>Wed, 18 May 2022 06:36:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-and-crystal-less-USB0-operation-in-device-mode/m-p/1459754#M48808</guid>
      <dc:creator>giusloq</dc:creator>
      <dc:date>2022-05-18T06:36:22Z</dc:date>
    </item>
    <item>
      <title>Re: LPC546xx and crystal-less USB0 operation in device mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-and-crystal-less-USB0-operation-in-device-mode/m-p/1459871#M48811</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;You can download it from the link:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/TN00032.zip" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/TN00032.zip&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;If you can not download it, pls update the ticket, I will attach it here.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 18 May 2022 08:39:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-and-crystal-less-USB0-operation-in-device-mode/m-p/1459871#M48811</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-05-18T08:39:38Z</dc:date>
    </item>
  </channel>
</rss>