<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: How many PMSM motors can the LPC553x run?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-many-PMSM-motors-can-the-LPC553x-run/m-p/1454746#M48693</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;If you use LPC553x to control PMSM or BLDC, for each LPC553x,&amp;nbsp; there are two eFlxPWM modules, two ENC modules(which can decode Encoder signal to get rotor position), two ADC modules, so each LPC553x can control two motors, in other words, the two motors can be&amp;nbsp; two PMSM,&amp;nbsp; two BLDC,&amp;nbsp; or one PMSM and one BLDC.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
    <pubDate>Mon, 09 May 2022 06:18:04 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2022-05-09T06:18:04Z</dc:date>
    <item>
      <title>How many PMSM motors can the LPC553x run?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-many-PMSM-motors-can-the-LPC553x-run/m-p/1454538#M48687</link>
      <description>&lt;P&gt;I've seen the motor demo with the LPC553x. Curious if there has been any tests done on the total qty of &amp;nbsp;BLDC/PMSM motors on IC could run!?&lt;/P&gt;</description>
      <pubDate>Sun, 08 May 2022 12:17:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-many-PMSM-motors-can-the-LPC553x-run/m-p/1454538#M48687</guid>
      <dc:creator>dav1</dc:creator>
      <dc:date>2022-05-08T12:17:58Z</dc:date>
    </item>
    <item>
      <title>Re: How many PMSM motors can the LPC553x run?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-many-PMSM-motors-can-the-LPC553x-run/m-p/1454746#M48693</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;If you use LPC553x to control PMSM or BLDC, for each LPC553x,&amp;nbsp; there are two eFlxPWM modules, two ENC modules(which can decode Encoder signal to get rotor position), two ADC modules, so each LPC553x can control two motors, in other words, the two motors can be&amp;nbsp; two PMSM,&amp;nbsp; two BLDC,&amp;nbsp; or one PMSM and one BLDC.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Mon, 09 May 2022 06:18:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-many-PMSM-motors-can-the-LPC553x-run/m-p/1454746#M48693</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-05-09T06:18:04Z</dc:date>
    </item>
  </channel>
</rss>