<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC82x v2/mbed MCUXpresso SDK Multi Timer Blinky Example in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82x-v2-mbed-MCUXpresso-SDK-Multi-Timer-Blinky-Example/m-p/1446626#M48517</link>
    <description>&lt;P&gt;Hi Everyone,&lt;/P&gt;&lt;P&gt;I'm completely new to developing and I was running into some problems getting the Multi Timer Blinky example to work on the LPC82x board.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The project is straight from the SDK provided from NXP.&amp;nbsp; It can build without error, but when I try to run it, I receive this error message (MCUXpresso Error.PNG).&amp;nbsp; I have my board connected to my PC and the LED is lit, so I know there is power on the board.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;These are the things I tried to do:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;hit the "Clean Up Debug" button on the IDE, power cycle the board and try again.&amp;nbsp;&lt;/LI&gt;&lt;LI&gt;switch USB cables&lt;/LI&gt;&lt;LI&gt;use a different PC&lt;/LI&gt;&lt;LI&gt;&amp;nbsp;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Here is a List of Materials:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;LPC82x Xpresso v2/mbed&lt;/LI&gt;&lt;LI&gt;USB cable&lt;/LI&gt;&lt;LI&gt;Windows 10 Pro verison:21H1&lt;/LI&gt;&lt;LI&gt;MCUXpressoIDE_11.5.0_7232&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I just don't understand why I'm failing to run the simplest of programs D;&lt;BR /&gt;Any help would be greatly appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Justin&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 20 Apr 2022 19:16:31 GMT</pubDate>
    <dc:creator>Justin_S</dc:creator>
    <dc:date>2022-04-20T19:16:31Z</dc:date>
    <item>
      <title>LPC82x v2/mbed MCUXpresso SDK Multi Timer Blinky Example</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82x-v2-mbed-MCUXpresso-SDK-Multi-Timer-Blinky-Example/m-p/1446626#M48517</link>
      <description>&lt;P&gt;Hi Everyone,&lt;/P&gt;&lt;P&gt;I'm completely new to developing and I was running into some problems getting the Multi Timer Blinky example to work on the LPC82x board.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The project is straight from the SDK provided from NXP.&amp;nbsp; It can build without error, but when I try to run it, I receive this error message (MCUXpresso Error.PNG).&amp;nbsp; I have my board connected to my PC and the LED is lit, so I know there is power on the board.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;These are the things I tried to do:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;hit the "Clean Up Debug" button on the IDE, power cycle the board and try again.&amp;nbsp;&lt;/LI&gt;&lt;LI&gt;switch USB cables&lt;/LI&gt;&lt;LI&gt;use a different PC&lt;/LI&gt;&lt;LI&gt;&amp;nbsp;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Here is a List of Materials:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;LPC82x Xpresso v2/mbed&lt;/LI&gt;&lt;LI&gt;USB cable&lt;/LI&gt;&lt;LI&gt;Windows 10 Pro verison:21H1&lt;/LI&gt;&lt;LI&gt;MCUXpressoIDE_11.5.0_7232&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I just don't understand why I'm failing to run the simplest of programs D;&lt;BR /&gt;Any help would be greatly appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Justin&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 20 Apr 2022 19:16:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82x-v2-mbed-MCUXpresso-SDK-Multi-Timer-Blinky-Example/m-p/1446626#M48517</guid>
      <dc:creator>Justin_S</dc:creator>
      <dc:date>2022-04-20T19:16:31Z</dc:date>
    </item>
    <item>
      <title>Re: LPC82x v2/mbed MCUXpresso SDK Multi Timer Blinky Example</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82x-v2-mbed-MCUXpresso-SDK-Multi-Timer-Blinky-Example/m-p/1446837#M48520</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Pls try to hold the SW2 button , then insert USB to power up the board, then release the SW2, then try to download code.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Thu, 21 Apr 2022 02:02:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82x-v2-mbed-MCUXpresso-SDK-Multi-Timer-Blinky-Example/m-p/1446837#M48520</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-04-21T02:02:32Z</dc:date>
    </item>
    <item>
      <title>Re: LPC82x v2/mbed MCUXpresso SDK Multi Timer Blinky Example</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82x-v2-mbed-MCUXpresso-SDK-Multi-Timer-Blinky-Example/m-p/1449383#M48567</link>
      <description>&lt;P&gt;Hi XiangJun,&lt;/P&gt;&lt;P&gt;So I did what you suggested, but I still run into the previous error.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I try to debug, this is the error I receive, I've attached a pic.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Side note, when I plug in my board to my laptop, should I be able to see my COM port in device manager?&amp;nbsp; I've tried every port in my laptop, and the COM never shows up, I have to select "show hidden devices" in order to see the device manager pic I attached.&amp;nbsp; Should it matter?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Justin&lt;/P&gt;</description>
      <pubDate>Tue, 26 Apr 2022 18:50:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82x-v2-mbed-MCUXpresso-SDK-Multi-Timer-Blinky-Example/m-p/1449383#M48567</guid>
      <dc:creator>Justin_S</dc:creator>
      <dc:date>2022-04-26T18:50:16Z</dc:date>
    </item>
    <item>
      <title>Re: LPC82x v2/mbed MCUXpresso SDK Multi Timer Blinky Example</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82x-v2-mbed-MCUXpresso-SDK-Multi-Timer-Blinky-Example/m-p/1449701#M48572</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I suggest you download Flashmagic from the link:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.flashmagictool.com/" target="_blank"&gt;https://www.flashmagictool.com/&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Pls insert USB cable while you hold the SW2(ISP pin), then release SW2, the chip will enter boot mode. Try to use flashmagic tools to download&lt;/P&gt;
&lt;P&gt;Regarding your error that you can not download code via SWD, I do not know, maybe the board has broken down.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Wed, 27 Apr 2022 07:08:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82x-v2-mbed-MCUXpresso-SDK-Multi-Timer-Blinky-Example/m-p/1449701#M48572</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-04-27T07:08:46Z</dc:date>
    </item>
  </channel>
</rss>