<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Can LPC55S69 run 1.8V GPIO/UART ? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-LPC55S69-run-1-8V-GPIO-UART/m-p/1445605#M48505</link>
    <description>&lt;P&gt;Hi&amp;nbsp;dav1&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes&amp;nbsp;&lt;SPAN&gt;LPC55S69 VDD&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;absolute minimum is 1.8V. We can guarantee the part work safe with 1.8V.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;We can't guarantee operation&amp;nbsp;normal with&amp;nbsp;&amp;nbsp;1.72V VDD.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Jun Zhang&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 19 Apr 2022 09:14:09 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2022-04-19T09:14:09Z</dc:date>
    <item>
      <title>Can LPC55S69 run 1.8V GPIO/UART ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-LPC55S69-run-1-8V-GPIO-UART/m-p/1444617#M48490</link>
      <description>&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;The datasheet for LPC55S69JEV98K states VDD 'main io supply', min 1.8V&lt;/P&gt;&lt;P&gt;does that mean 1.800V ?&amp;nbsp;&lt;BR /&gt;i.e. most buck regulators would have about 3-5% output tolerance, meaning the VDD rail and serial IO might as well be 1.72V.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is the datasheet correct, i.e. 1.8V is absolute minimum? or can you run the LPC55-series safely in a 1.8V system?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thx&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 15 Apr 2022 14:07:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-LPC55S69-run-1-8V-GPIO-UART/m-p/1444617#M48490</guid>
      <dc:creator>dav1</dc:creator>
      <dc:date>2022-04-15T14:07:54Z</dc:date>
    </item>
    <item>
      <title>Re: Can LPC55S69 run 1.8V GPIO/UART ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-LPC55S69-run-1-8V-GPIO-UART/m-p/1445605#M48505</link>
      <description>&lt;P&gt;Hi&amp;nbsp;dav1&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes&amp;nbsp;&lt;SPAN&gt;LPC55S69 VDD&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;absolute minimum is 1.8V. We can guarantee the part work safe with 1.8V.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;We can't guarantee operation&amp;nbsp;normal with&amp;nbsp;&amp;nbsp;1.72V VDD.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Jun Zhang&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 19 Apr 2022 09:14:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-LPC55S69-run-1-8V-GPIO-UART/m-p/1445605#M48505</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2022-04-19T09:14:09Z</dc:date>
    </item>
  </channel>
</rss>