<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Booting LPC55 via I2C, can we trigger flash-boot via rom-loader?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Booting-LPC55-via-I2C-can-we-trigger-flash-boot-via-rom-loader/m-p/1445528#M48504</link>
    <description>&lt;P&gt;thanks, sounds good!&lt;/P&gt;&lt;P&gt;do you have an idea of how long it will take to run these commands over i2c?&lt;/P&gt;&lt;P&gt;i couldn't find any wait times in the datasheet so should be fairly instant (i hope)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 19 Apr 2022 07:53:40 GMT</pubDate>
    <dc:creator>dav1</dc:creator>
    <dc:date>2022-04-19T07:53:40Z</dc:date>
    <item>
      <title>Booting LPC55 via I2C, can we trigger flash-boot via rom-loader?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Booting-LPC55-via-I2C-can-we-trigger-flash-boot-via-rom-loader/m-p/1444626#M48491</link>
      <description>&lt;P&gt;When using the built-in I2C "ISP boot mode" of the&amp;nbsp;LPC55 series cpu's&lt;BR /&gt;&lt;SPAN&gt;is it possible for the host to signal via I2C to immediately exit the rom based bootloader to continue booting via flash?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I don't have the option to add a dedicated gpio to control ISP, so idea was to always enter the rom boot mode -&amp;gt; read flash region to check installed firmware -&amp;gt; if up to date -&amp;gt; continue to boot via flash&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;doable?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 15 Apr 2022 14:45:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Booting-LPC55-via-I2C-can-we-trigger-flash-boot-via-rom-loader/m-p/1444626#M48491</guid>
      <dc:creator>dav1</dc:creator>
      <dc:date>2022-04-15T14:45:25Z</dc:date>
    </item>
    <item>
      <title>Re: Booting LPC55 via I2C, can we trigger flash-boot via rom-loader?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Booting-LPC55-via-I2C-can-we-trigger-flash-boot-via-rom-loader/m-p/1444875#M48493</link>
      <description>&lt;P&gt;Yes, you can try read-memory and execute commands in UM 8.9.5 I2C ISP commands&lt;/P&gt;
&lt;P&gt;Use read-memory command to read back app data from internal flash&lt;/P&gt;
&lt;P&gt;Use execute command to jump to app&lt;/P&gt;</description>
      <pubDate>Mon, 18 Apr 2022 04:50:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Booting-LPC55-via-I2C-can-we-trigger-flash-boot-via-rom-loader/m-p/1444875#M48493</guid>
      <dc:creator>jay_heng</dc:creator>
      <dc:date>2022-04-18T04:50:26Z</dc:date>
    </item>
    <item>
      <title>Re: Booting LPC55 via I2C, can we trigger flash-boot via rom-loader?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Booting-LPC55-via-I2C-can-we-trigger-flash-boot-via-rom-loader/m-p/1445528#M48504</link>
      <description>&lt;P&gt;thanks, sounds good!&lt;/P&gt;&lt;P&gt;do you have an idea of how long it will take to run these commands over i2c?&lt;/P&gt;&lt;P&gt;i couldn't find any wait times in the datasheet so should be fairly instant (i hope)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 19 Apr 2022 07:53:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Booting-LPC55-via-I2C-can-we-trigger-flash-boot-via-rom-loader/m-p/1445528#M48504</guid>
      <dc:creator>dav1</dc:creator>
      <dc:date>2022-04-19T07:53:40Z</dc:date>
    </item>
    <item>
      <title>Re: Booting LPC55 via I2C, can we trigger flash-boot via rom-loader?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Booting-LPC55-via-I2C-can-we-trigger-flash-boot-via-rom-loader/m-p/1581813#M51263</link>
      <description>&lt;P&gt;having trouble with this, the UM 8.9.5 doesn't have an example so tried this:&lt;/P&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;boot_cmd[22] = {0x5A,0xA4,0x10,0x00,0x00,0x00,&lt;STRONG&gt;0x09&lt;/STRONG&gt;,0x00,0x00,0x03,0x6c,0x01,0x00,0x00,0x00,0x80,0x01,0x20,0x00,0x80,0x01,0x20}&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;where 0x09 is the execute cmd, but the response code is command not supported&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Thu, 12 Jan 2023 15:04:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Booting-LPC55-via-I2C-can-we-trigger-flash-boot-via-rom-loader/m-p/1581813#M51263</guid>
      <dc:creator>dav1</dc:creator>
      <dc:date>2023-01-12T15:04:41Z</dc:date>
    </item>
  </channel>
</rss>