<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: video on lpc1788. Is it possible?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/video-on-lpc1788-Is-it-possible/m-p/522209#M4845</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ktownsend on Sun Mar 11 18:45:36 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;You'll need to provide more information to offer a meaningful answer to that question.&amp;nbsp; It depends on the width of your memory (16 or 32-bit), the size of your LCD (320x240 isn't very demanding, but 800x480 is very taxing on the system), the screen refresh rate and not just the video framerate.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If you are using a 320x240 LCD and 320x240 video, it may be possible, but there are far to many variables involved to be able to provide a useful answer on if it's possible or not.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:54:42 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:54:42Z</dc:date>
    <item>
      <title>video on lpc1788. Is it possible?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/video-on-lpc1788-Is-it-possible/m-p/522208#M4844</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by siriasis on Sun Mar 11 16:47:26 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Guys, Is it possible to run video on LPC1788. 15fps. Has anyone tried anything like this on this chip. Video information will come from external networking camera.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance &lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:54:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/video-on-lpc1788-Is-it-possible/m-p/522208#M4844</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:54:41Z</dc:date>
    </item>
    <item>
      <title>Re: video on lpc1788. Is it possible?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/video-on-lpc1788-Is-it-possible/m-p/522209#M4845</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ktownsend on Sun Mar 11 18:45:36 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;You'll need to provide more information to offer a meaningful answer to that question.&amp;nbsp; It depends on the width of your memory (16 or 32-bit), the size of your LCD (320x240 isn't very demanding, but 800x480 is very taxing on the system), the screen refresh rate and not just the video framerate.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If you are using a 320x240 LCD and 320x240 video, it may be possible, but there are far to many variables involved to be able to provide a useful answer on if it's possible or not.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:54:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/video-on-lpc1788-Is-it-possible/m-p/522209#M4845</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:54:42Z</dc:date>
    </item>
  </channel>
</rss>