<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: NXP PN512 working with IRQ</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/NXP-PN512-working-with-IRQ/m-p/1433227#M48325</link>
    <description>&lt;P&gt;None of examples is using IRQ line from PN512. Function&amp;nbsp;&lt;SPAN&gt;phacDiscLoop_Run is waiting until all instruction are done. So you can't do anything else during this time. Maybe there is some example based on interrupts, but I can't find it.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 24 Mar 2022 06:50:39 GMT</pubDate>
    <dc:creator>januszjonski</dc:creator>
    <dc:date>2022-03-24T06:50:39Z</dc:date>
    <item>
      <title>NXP PN512 working with IRQ</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/NXP-PN512-working-with-IRQ/m-p/1431290#M48285</link>
      <description>&lt;P&gt;HI,&lt;/P&gt;&lt;P&gt;I want to use NxpRdLib in order to create mifare card reader using module PN512. All functions works fine under LPC1519JBD100e, but my program is blocked for 250 - 380 ms when I run function "status = phacDiscLoop_Run(&amp;amp;sDiscLoop, wEntryPoint);".&amp;nbsp;&lt;/P&gt;&lt;P&gt;How can I configure PN512 to receive no-blocking communication. Is there any example.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 21 Mar 2022 12:21:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/NXP-PN512-working-with-IRQ/m-p/1431290#M48285</guid>
      <dc:creator>januszjonski</dc:creator>
      <dc:date>2022-03-21T12:21:44Z</dc:date>
    </item>
    <item>
      <title>Re: NXP PN512 working with IRQ</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/NXP-PN512-working-with-IRQ/m-p/1433096#M48322</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;It is hard to know the root cause from your description, you can trace into function&amp;nbsp;&lt;SPAN&gt;phacDiscLoop_Run.&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;There is a Ex10 demo for MIFARE DESFire. It is under NDA.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Thu, 24 Mar 2022 03:44:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/NXP-PN512-working-with-IRQ/m-p/1433096#M48322</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2022-03-24T03:44:00Z</dc:date>
    </item>
    <item>
      <title>Re: NXP PN512 working with IRQ</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/NXP-PN512-working-with-IRQ/m-p/1433227#M48325</link>
      <description>&lt;P&gt;None of examples is using IRQ line from PN512. Function&amp;nbsp;&lt;SPAN&gt;phacDiscLoop_Run is waiting until all instruction are done. So you can't do anything else during this time. Maybe there is some example based on interrupts, but I can't find it.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 24 Mar 2022 06:50:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/NXP-PN512-working-with-IRQ/m-p/1433227#M48325</guid>
      <dc:creator>januszjonski</dc:creator>
      <dc:date>2022-03-24T06:50:39Z</dc:date>
    </item>
  </channel>
</rss>