<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックMCUXpresso patch libraries</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/MCUXpresso-patch-libraries/m-p/1432611#M48315</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm using MCUXpresso to generate code and to include libraries etc needed for the project. However I need to patch one of the libraries (in this case fatfs to add another driver). As soon as I regenerate the project the patched files are overwritten. Is there any elegant way of handling this or should I give up and make a copy of fatfs that I can manage myself?&lt;/P&gt;&lt;P&gt;Thanks&lt;BR /&gt;/Björn&lt;/P&gt;</description>
    <pubDate>Wed, 23 Mar 2022 13:19:00 GMT</pubDate>
    <dc:creator>bjorns</dc:creator>
    <dc:date>2022-03-23T13:19:00Z</dc:date>
    <item>
      <title>MCUXpresso patch libraries</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/MCUXpresso-patch-libraries/m-p/1432611#M48315</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm using MCUXpresso to generate code and to include libraries etc needed for the project. However I need to patch one of the libraries (in this case fatfs to add another driver). As soon as I regenerate the project the patched files are overwritten. Is there any elegant way of handling this or should I give up and make a copy of fatfs that I can manage myself?&lt;/P&gt;&lt;P&gt;Thanks&lt;BR /&gt;/Björn&lt;/P&gt;</description>
      <pubDate>Wed, 23 Mar 2022 13:19:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/MCUXpresso-patch-libraries/m-p/1432611#M48315</guid>
      <dc:creator>bjorns</dc:creator>
      <dc:date>2022-03-23T13:19:00Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso patch libraries</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/MCUXpresso-patch-libraries/m-p/1435406#M48358</link>
      <description>&lt;P&gt;Hello &lt;SPAN class="UserName lia-user-name lia-user-rank-Contributor-II lia-component-message-view-widget-author-username"&gt;&lt;A id="link_12" class="lia-link-navigation lia-page-link lia-user-name-link" style="color: #333f48;" href="https://community.nxp.com/t5/user/viewprofilepage/user-id/196708" target="_self" aria-label="View Profile of bjorns"&gt;&lt;SPAN class=""&gt;bjorns&lt;/SPAN&gt;&lt;/A&gt;&lt;/SPAN&gt;,&lt;/P&gt;
&lt;P&gt;The configuration files for pins, clocks and peripherals are fully generated by the config tools. The user should use MCUXPresso config tools user interface to make any changes and the re-generate the code. It’s not supported to do manual changes in the generated files.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Tue, 29 Mar 2022 08:52:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/MCUXpresso-patch-libraries/m-p/1435406#M48358</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2022-03-29T08:52:30Z</dc:date>
    </item>
  </channel>
</rss>