<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: emwin window manager paint parrent when create new window in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/emwin-window-manager-paint-parrent-when-create-new-window/m-p/1430912#M48274</link>
    <description>&lt;P&gt;I utilise scrollbars because they eliminate the need for buttons on the left and right sides of a slider to increase and decrement the slider. The scrollbar also has an auto-repeat option built in. I skinned the scrollbar properly, and I can now print values within the thumb. They are, for the most part, highly effective. Having said that, I did had that issue, which looks to be resolved by adding the GUI Exec command ().&lt;/P&gt;&lt;P&gt;Yeah, it's definitely not the ideal method, but I'd been working with sliders for months and decided this was a nicer aesthetic, plus the scrollbar added to the product's usefulness.&lt;/P&gt;</description>
    <pubDate>Sat, 19 Mar 2022 12:47:40 GMT</pubDate>
    <dc:creator>JefferyOlsen</dc:creator>
    <dc:date>2022-03-19T12:47:40Z</dc:date>
    <item>
      <title>emwin window manager paint parrent when create new window</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/emwin-window-manager-paint-parrent-when-create-new-window/m-p/633249#M24942</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi everyone i have a problem in emwin&lt;/P&gt;&lt;P&gt;my program contains some framewin that open one in another(means they are modal and open as child of others)&lt;/P&gt;&lt;P&gt;in each framewin i have some widget contains an image as background when i open new framewin in another framewin&lt;/P&gt;&lt;P&gt;the paint message of parent runs ,this process make the program heavy and &lt;SPAN&gt;consequently&lt;/SPAN&gt; flicker effect&lt;/P&gt;&lt;P&gt;my question is that how to avoid parent window repaint when another window cover its area completely&lt;/P&gt;&lt;P&gt;thanks in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Dec 2016 13:25:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/emwin-window-manager-paint-parrent-when-create-new-window/m-p/633249#M24942</guid>
      <dc:creator>dolphinapadana</dc:creator>
      <dc:date>2016-12-21T13:25:03Z</dc:date>
    </item>
    <item>
      <title>Re: emwin window manager paint parrent when create new window</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/emwin-window-manager-paint-parrent-when-create-new-window/m-p/1430912#M48274</link>
      <description>&lt;P&gt;I utilise scrollbars because they eliminate the need for buttons on the left and right sides of a slider to increase and decrement the slider. The scrollbar also has an auto-repeat option built in. I skinned the scrollbar properly, and I can now print values within the thumb. They are, for the most part, highly effective. Having said that, I did had that issue, which looks to be resolved by adding the GUI Exec command ().&lt;/P&gt;&lt;P&gt;Yeah, it's definitely not the ideal method, but I'd been working with sliders for months and decided this was a nicer aesthetic, plus the scrollbar added to the product's usefulness.&lt;/P&gt;</description>
      <pubDate>Sat, 19 Mar 2022 12:47:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/emwin-window-manager-paint-parrent-when-create-new-window/m-p/1430912#M48274</guid>
      <dc:creator>JefferyOlsen</dc:creator>
      <dc:date>2022-03-19T12:47:40Z</dc:date>
    </item>
  </channel>
</rss>