<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Trouble Reading/Writing data on external SPI flash  W25Q80DV on LPC54016 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Trouble-Reading-Writing-data-on-external-SPI-flash-W25Q80DV-on/m-p/1428605#M48233</link>
    <description>&lt;P&gt;So if I want to write some data in external SPI flash it should be written starting from 0x4000_0000?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a reason why I am getting an error while writing the data buffer and I get that "Failed to execute MI command"? It says cannot access at address 0x40080014 because I have "??" there.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is what I have set in the code,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;/** Peripheral SPIFI0 base address */&lt;BR /&gt;#define SPIFI0_BASE (0x40080000u)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is where I write all the data and command.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;/* @brief SPIFI start address */&lt;BR /&gt;#define FSL_FEATURE_SPIFI_START_ADDR (0x10000000)&lt;BR /&gt;uint8_t *val = (uint8_t *)FSL_FEATURE_SPIFI_START_ADDR;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is where I read the written data.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using the sdk example "SPIFI polling transfer" as it is.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It would be really helpful if you tell me if I am not doing anything right in these definitions or I need to use a different sdk example.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 15 Mar 2022 15:06:20 GMT</pubDate>
    <dc:creator>NVazquez</dc:creator>
    <dc:date>2022-03-15T15:06:20Z</dc:date>
    <item>
      <title>Trouble Reading/Writing data on external SPI flash  W25Q80DV on LPC54016</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Trouble-Reading-Writing-data-on-external-SPI-flash-W25Q80DV-on/m-p/1426349#M48173</link>
      <description>&lt;P&gt;I am using "spifi_polling_transfer" sdk example on a custom board for lpc54016 with winbond w25Q80DV.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have few beginners questions,&lt;/P&gt;&lt;P&gt;1. How can I view the data for external SPI Flash on MCUxpresso IDE 11.5.0? I tried using "memory tab" not sure if that's the RAM or External SPI flash.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;2. The base address defined is,&amp;nbsp;0x40080000u.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;/** Peripheral SPIFI0 base address */&lt;BR /&gt;#define SPIFI0_BASE (0x40080000u)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does that means this is the address we start writing the data?&lt;/P&gt;&lt;P&gt;3. The start address defines is&amp;nbsp;(0x10000000)&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;#define FSL_FEATURE_SPIFI_START_ADDR (0x10000000)&lt;/P&gt;&lt;P&gt;This is where we read the data we wrote, why does this address not match with SPIFI0 base address?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;4. where I fill the buffer&lt;/P&gt;&lt;P&gt;/* Set the buffer */&lt;BR /&gt;for (i = 0; i &amp;lt; PAGE_SIZE; i++)&lt;BR /&gt;{&lt;BR /&gt;g_buffer[i] = i;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;5. I am using the sample sdk example as it is, do I need to change anything? the sample code used W25Q128JV.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am trying to use the external flash to store the code memory as well as store some data.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/26034"&gt;@xiangjun_rong&lt;/a&gt;&amp;nbsp;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/13026"&gt;@ZhangJennie&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;the location where this data is written is always 0x20000048. Why is that? Is this the RAM location or external SPI flash.&lt;/P&gt;</description>
      <pubDate>Thu, 10 Mar 2022 18:54:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Trouble-Reading-Writing-data-on-external-SPI-flash-W25Q80DV-on/m-p/1426349#M48173</guid>
      <dc:creator>NVazquez</dc:creator>
      <dc:date>2022-03-10T18:54:44Z</dc:date>
    </item>
    <item>
      <title>Re: Trouble Reading/Writing data on external SPI flash  W25Q80DV on LPC54016</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Trouble-Reading-Writing-data-on-external-SPI-flash-W25Q80DV-on/m-p/1426397#M48174</link>
      <description>&lt;P&gt;I tried to debug, I think due to some reason my data is not getting written,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="NVazquez_0-1646950163340.png" style="width: 895px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/173113iF82E299DF2F62002/image-dimensions/895x611?v=v2" width="895" height="611" role="button" title="NVazquez_0-1646950163340.png" alt="NVazquez_0-1646950163340.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;NVazquez_0-1646950163340.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;this is what I'm getting.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;some screen shots if that's going to help understand my problem,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="NVazquez_1-1646950256424.png" style="width: 888px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/173114i5F91793354B36E8C/image-dimensions/888x484?v=v2" width="888" height="484" role="button" title="NVazquez_1-1646950256424.png" alt="NVazquez_1-1646950256424.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;NVazquez_1-1646950256424.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="NVazquez_2-1646950277862.png" style="width: 948px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/173115i8B315C724771219D/image-dimensions/948x988?v=v2" width="948" height="988" role="button" title="NVazquez_2-1646950277862.png" alt="NVazquez_2-1646950277862.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;NVazquez_2-1646950277862.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 10 Mar 2022 22:12:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Trouble-Reading-Writing-data-on-external-SPI-flash-W25Q80DV-on/m-p/1426397#M48174</guid>
      <dc:creator>NVazquez</dc:creator>
      <dc:date>2022-03-10T22:12:05Z</dc:date>
    </item>
    <item>
      <title>Re: Trouble Reading/Writing data on external SPI flash  W25Q80DV on LPC54016</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Trouble-Reading-Writing-data-on-external-SPI-flash-W25Q80DV-on/m-p/1426412#M48176</link>
      <description>&lt;P&gt;static inline void CLOCK_EnableClock(clock_ip_name_t clk)&lt;BR /&gt;{&lt;BR /&gt;uint32_t index = CLK_GATE_ABSTRACT_REG_OFFSET(clk);&lt;BR /&gt;if (index &amp;lt; 3UL)&lt;BR /&gt;{&lt;BR /&gt;SYSCON-&amp;gt;AHBCLKCTRLSET[index] = (1UL &amp;lt;&amp;lt; CLK_GATE_ABSTRACT_BITS_SHIFT(clk));&lt;BR /&gt;}&lt;BR /&gt;else&lt;BR /&gt;{&lt;BR /&gt;SYSCON-&amp;gt;ASYNCAPBCTRL = SYSCON_ASYNCAPBCTRL_ENABLE(1);&lt;BR /&gt;ASYNC_SYSCON-&amp;gt;ASYNCAPBCLKCTRLSET = (1UL &amp;lt;&amp;lt; CLK_GATE_ABSTRACT_BITS_SHIFT(clk));&lt;BR /&gt;}&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried to debug exactly where I get question marks at 40080000 location and it looks like, when I execute this line "SYSCON-&amp;gt;AHBCLKCTRLSET[index] = (1UL &amp;lt;&amp;lt; CLK_GATE_ABSTRACT_BITS_SHIFT(clk));".&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a 12Mhz crystal on my board, do I need to make some changes in the sample sdk code?&lt;/P&gt;</description>
      <pubDate>Thu, 10 Mar 2022 23:42:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Trouble-Reading-Writing-data-on-external-SPI-flash-W25Q80DV-on/m-p/1426412#M48176</guid>
      <dc:creator>NVazquez</dc:creator>
      <dc:date>2022-03-10T23:42:50Z</dc:date>
    </item>
    <item>
      <title>Re: Trouble Reading/Writing data on external SPI flash  W25Q80DV on LPC54016</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Trouble-Reading-Writing-data-on-external-SPI-flash-W25Q80DV-on/m-p/1427482#M48200</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Pls refer to the memory map of LPC546xx in UM11060.pdf, as you see that the base address 0x1000_0000 is spifi flash start address, the 0x2000_0000 is on-chip RAM address, the 0x4000_0000 is peripheral register address.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1647236944210.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/173467i5F289A02CE656621/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1647236944210.png" alt="xiangjun_rong_0-1647236944210.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;xiangjun_rong_0-1647236944210.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 14 Mar 2022 05:53:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Trouble-Reading-Writing-data-on-external-SPI-flash-W25Q80DV-on/m-p/1427482#M48200</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-03-14T05:53:46Z</dc:date>
    </item>
    <item>
      <title>Re: Trouble Reading/Writing data on external SPI flash  W25Q80DV on LPC54016</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Trouble-Reading-Writing-data-on-external-SPI-flash-W25Q80DV-on/m-p/1428605#M48233</link>
      <description>&lt;P&gt;So if I want to write some data in external SPI flash it should be written starting from 0x4000_0000?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a reason why I am getting an error while writing the data buffer and I get that "Failed to execute MI command"? It says cannot access at address 0x40080014 because I have "??" there.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is what I have set in the code,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;/** Peripheral SPIFI0 base address */&lt;BR /&gt;#define SPIFI0_BASE (0x40080000u)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is where I write all the data and command.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;/* @brief SPIFI start address */&lt;BR /&gt;#define FSL_FEATURE_SPIFI_START_ADDR (0x10000000)&lt;BR /&gt;uint8_t *val = (uint8_t *)FSL_FEATURE_SPIFI_START_ADDR;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is where I read the written data.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using the sdk example "SPIFI polling transfer" as it is.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It would be really helpful if you tell me if I am not doing anything right in these definitions or I need to use a different sdk example.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 15 Mar 2022 15:06:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Trouble-Reading-Writing-data-on-external-SPI-flash-W25Q80DV-on/m-p/1428605#M48233</guid>
      <dc:creator>NVazquez</dc:creator>
      <dc:date>2022-03-15T15:06:20Z</dc:date>
    </item>
    <item>
      <title>Re: Trouble Reading/Writing data on external SPI flash  W25Q80DV on LPC54016</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Trouble-Reading-Writing-data-on-external-SPI-flash-W25Q80DV-on/m-p/1429986#M48252</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I have to say that the address 0x4000_0000 are peripheral register address, they have special meaning for each register, you can NOT write them as general memory.&lt;/P&gt;
&lt;P&gt;For the spifi flash writing example project "spifi_polling_transfer",&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;/* Write enable */&lt;BR /&gt;SPIFI_SetCommand(EXAMPLE_SPIFI, &amp;amp;command[WRITE_ENABLE]);&lt;BR /&gt;/* Set address */&lt;BR /&gt;SPIFI_SetCommandAddress(EXAMPLE_SPIFI, 0U);&lt;/P&gt;
&lt;P&gt;//Rong write:&lt;/P&gt;
&lt;P&gt;the address 0 is the external spifi flash offset, it's absolute address is 0x1000_0000 in the ARM core address space, which also save application code, so if your write address, the application code is overwritten. You have to select an offset which does not occupy with application code so that you can put your application data to the space.&lt;/P&gt;
&lt;P&gt;For the program part code, it is the same that the address is the offset of external flash rather than absolute address.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;/* Erase sector */&lt;BR /&gt;SPIFI_SetCommand(EXAMPLE_SPIFI, &amp;amp;command[ERASE_SECTOR]);&lt;BR /&gt;/* Check if finished */&lt;BR /&gt;check_if_finish();&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 17 Mar 2022 09:11:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Trouble-Reading-Writing-data-on-external-SPI-flash-W25Q80DV-on/m-p/1429986#M48252</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-03-17T09:11:02Z</dc:date>
    </item>
    <item>
      <title>Re: Trouble Reading/Writing data on external SPI flash  W25Q80DV on LPC54016</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Trouble-Reading-Writing-data-on-external-SPI-flash-W25Q80DV-on/m-p/1430229#M48259</link>
      <description>&lt;P&gt;I tried to run the "&lt;SPAN&gt;"spifi_polling_transfer"" code on EVK 540s0xx board and it works perfect.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Not sure why it does work on my custom board with controller LPC54016 and the winbond I am using is W25Q80DV.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I am able to read the memory and erase it successfully but when I try to write it, it writes from 0x10000000 to 0x17FFFFFF location.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="NVazquez_0-1647534370094.png" style="width: 1155px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/174052iECC1CF2A0DBFACC2/image-dimensions/1155x378?v=v2" width="1155" height="378" role="button" title="NVazquez_0-1647534370094.png" alt="NVazquez_0-1647534370094.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;NVazquez_0-1647534370094.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried to check the frequency of SPIFI, by&amp;nbsp;&lt;BR /&gt;spifiFreq = CLOCK_GetSpifiClkFreq();&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and it is 96Mhz. Not sure if it is the configuration?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;#ifdef W25Q128JVFM&lt;BR /&gt;/* SPIFI Descriptor - W25Q128JVFM */&lt;BR /&gt;(void (*)(void))0x00000000, // 0xFFFFFFFF to default 1-bit SPI mode ；DevStrAdr&lt;BR /&gt;(void (*)(void))0x001870EF, // mfgId + extCount&lt;BR /&gt;(void (*)(void))0x00000000, // extid 0-3&lt;BR /&gt;(void (*)(void))0x00000000, // reserved&lt;BR /&gt;(void (*)(void))0x1301001D, // caps&lt;BR /&gt;(void (*)(void))0x00000100, // Blks + RESV1&lt;BR /&gt;(void (*)(void))0x00010000, // blkSize&lt;BR /&gt;(void (*)(void))0x00000000, // reserved&lt;BR /&gt;(void (*)(void))0x00000100, // pageSize + RESV2&lt;BR /&gt;(void (*)(void))0x00003F00, // maxReadSize&lt;BR /&gt;(void (*)(void))0x68506850, // maxClkRate,maxReadRate,maxHSReadRate,maxProgramRate&lt;BR /&gt;(void (*)(void))0x04030050, // maxHSProgramRate,initDeInitFxId,clearStatusFxId,getStatusFxId,&lt;BR /&gt;(void (*)(void))0x14110D09, // setStatusFxId,setOptionsFxId,getReadCmdFxId,getWriteCmdFxId&lt;BR /&gt;#endif&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do I need to change anything here?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If I am able to erase and read then I think the configuration is correct. Not sure what's going wrong with the write operation.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also I changed the Program page command from 31H to 01H according to the W25Q80 datasheet&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;//{1, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0x31}};&lt;BR /&gt;{1, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0x01}};&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any help will be appreciated.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 17 Mar 2022 16:31:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Trouble-Reading-Writing-data-on-external-SPI-flash-W25Q80DV-on/m-p/1430229#M48259</guid>
      <dc:creator>NVazquez</dc:creator>
      <dc:date>2022-03-17T16:31:27Z</dc:date>
    </item>
    <item>
      <title>Re: Trouble Reading/Writing data on external SPI flash  W25Q80DV on LPC54016</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Trouble-Reading-Writing-data-on-external-SPI-flash-W25Q80DV-on/m-p/1430840#M48271</link>
      <description>&lt;P&gt;I changed some of the configuration settings accoding to the datasheet for w25q80dv,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;(void (*)(void))0x001440EF, // mfgId + extCount for W25Q80DV&lt;BR /&gt;(void (*)(void))0x0000000F, // Blks + RESV1 for W25Q80DV&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I reduced the frequency to 49Mhz, 24Mhz still the garbage value is written in the flash W25Q80DV.&lt;/P&gt;&lt;P&gt;Works perfect on EVK56S0xx board. Attach the zip file for my code.&lt;/P&gt;</description>
      <pubDate>Fri, 18 Mar 2022 21:12:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Trouble-Reading-Writing-data-on-external-SPI-flash-W25Q80DV-on/m-p/1430840#M48271</guid>
      <dc:creator>NVazquez</dc:creator>
      <dc:date>2022-03-18T21:12:20Z</dc:date>
    </item>
    <item>
      <title>Re: Trouble Reading/Writing data on external SPI flash  W25Q80DV on LPC54016</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Trouble-Reading-Writing-data-on-external-SPI-flash-W25Q80DV-on/m-p/1432172#M48301</link>
      <description>&lt;P&gt;I am really struggling with reading/writing ext spi flash. Any help would be really appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I don't understand if I can read and write the same code "SPIFI polling transfer" on EVK board with 54S018 and W25Q128. Why can't I use the same software with 54016 with w25q80DV.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I reduced the frequency to 12Mhz, changed the configuration setting as per w25q80. Not sure what else I need to do.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Are there any hardware requirements?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How does the sample code checks if the JEDEC ID is correct?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is the config I am using,&lt;/P&gt;&lt;P&gt;&amp;nbsp;/* SPIFI Descriptor - W25Q80DVSIG */&lt;BR /&gt;(void (*)(void))0x00000000, // 0xFFFFFFFF to default 1-bit SPI mode ；DevStrAdr&lt;BR /&gt;(void (*)(void))0x001440EF, // mfgId + extCount for W25Q80DV&lt;BR /&gt;(void (*)(void))0x00000000, // extid 0-3&lt;BR /&gt;(void (*)(void))0x00000000, // reserved&lt;BR /&gt;(void (*)(void))0x1301001D, // caps&lt;BR /&gt;(void (*)(void))0x0000000F, // Blks + RESV1 for W25Q80DV&lt;BR /&gt;(void (*)(void))0x00010000, // blkSize&lt;BR /&gt;(void (*)(void))0x00000000, // reserved&lt;BR /&gt;(void (*)(void))0x00000100, // pageSize + RESV2&lt;BR /&gt;(void (*)(void))0x00003F00, // maxReadSize&lt;BR /&gt;(void (*)(void))0x68506850, // maxClkRate,maxReadRate,maxHSReadRate,maxProgramRate&lt;BR /&gt;(void (*)(void))0x04030050, // maxHSProgramRate,initDeInitFxId,clearStatusFxId,getStatusFxId,&lt;BR /&gt;(void (*)(void))0x14110D09, // setStatusFxId,setOptionsFxId,getReadCmdFxId,getWriteCmdFxId&lt;BR /&gt;#endif&lt;/P&gt;&lt;P&gt;Tried to use the chip as dual and quad mode, but still no luck.&lt;/P&gt;&lt;P&gt;There are not many post talking about communication with external SPI flash.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 22 Mar 2022 20:49:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Trouble-Reading-Writing-data-on-external-SPI-flash-W25Q80DV-on/m-p/1432172#M48301</guid>
      <dc:creator>NVazquez</dc:creator>
      <dc:date>2022-03-22T20:49:30Z</dc:date>
    </item>
    <item>
      <title>Re: Trouble Reading/Writing data on external SPI flash  W25Q80DV on LPC54016</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Trouble-Reading-Writing-data-on-external-SPI-flash-W25Q80DV-on/m-p/1435005#M48349</link>
      <description>&lt;P&gt;I was finally able to read and write w25q80dv chip using sample code for w25q128 "SPIFI polling transfer".&amp;nbsp;&lt;/P&gt;&lt;P&gt;I reduced the frequency to 12Mhz, change the configuration to,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;/* SPIFI Descriptor - W25Q80DVSIG */&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;(void (*)(void))0x00000000, // 0xFFFFFFFF to default 1-bit SPI mode ；DevStrAdr&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;(void (*)(void))0x001440EF, // mfgId + extCount for W25Q80DV&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;(void (*)(void))0x00000000, // extid 0-3&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;(void (*)(void))0x00000000, // reserved&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;(void (*)(void))0x1301001D, // caps&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;(void (*)(void))0x0000000F, // Blks + RESV1 for W25Q80DV&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;(void (*)(void))0x00010000, // blkSize&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;(void (*)(void))0x00000000, // reserved&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;(void (*)(void))0x00000100, // pageSize + RESV2&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;(void (*)(void))0x00003F00, // maxReadSize&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;(void (*)(void))0x68506850, // maxClkRate,maxReadRate,maxHSReadRate,maxProgramRate&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;(void (*)(void))0x04030050, // maxHSProgramRate,initDeInitFxId,clearStatusFxId,getStatusFxId,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;(void (*)(void))0x14110D09, // setStatusFxId,setOptionsFxId,getReadCmdFxId,getWriteCmdFxId&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#endif&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;and I had to give 16 data clock pulse after 8 clock pulse for write status register(01h). 6 clock pulse are for register 1 &amp;amp; register 2.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 28 Mar 2022 20:19:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Trouble-Reading-Writing-data-on-external-SPI-flash-W25Q80DV-on/m-p/1435005#M48349</guid>
      <dc:creator>NVazquez</dc:creator>
      <dc:date>2022-03-28T20:19:05Z</dc:date>
    </item>
  </channel>
</rss>