<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 lpc1768 EXTINT interface</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpc1768-EXTINT-interface/m-p/1428495#M48230</link>
    <description>&lt;P&gt;&lt;STRONG&gt;Hi,&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;I Try to config ir sensor in lpc1768 but it produce unwanted ripples&amp;nbsp;&lt;/STRONG&gt;&lt;STRONG&gt;so if i check the output connection should be active how to deactivated the output pin.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 15 Mar 2022 12:25:03 GMT</pubDate>
    <dc:creator>Sukumar_M</dc:creator>
    <dc:date>2022-03-15T12:25:03Z</dc:date>
    <item>
      <title>lpc1768 EXTINT interface</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpc1768-EXTINT-interface/m-p/1428495#M48230</link>
      <description>&lt;P&gt;&lt;STRONG&gt;Hi,&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;I Try to config ir sensor in lpc1768 but it produce unwanted ripples&amp;nbsp;&lt;/STRONG&gt;&lt;STRONG&gt;so if i check the output connection should be active how to deactivated the output pin.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 15 Mar 2022 12:25:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/lpc1768-EXTINT-interface/m-p/1428495#M48230</guid>
      <dc:creator>Sukumar_M</dc:creator>
      <dc:date>2022-03-15T12:25:03Z</dc:date>
    </item>
    <item>
      <title>Re: lpc1768 EXTINT interface</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpc1768-EXTINT-interface/m-p/1428882#M48239</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;As you know that the uart can transmit irDa signal from it's Uartx_TX pin, which is a bit stream modulated by the 38KHz signal, the 38khz fixed duty cycle signal can be generated by uart module itself. If you want LPC uart_rx pin to receive the irDa signal, I suppose that you have to create an analog low-pass filter circuit to remove the 38K modulated signal, then use uart_RX pin to receive the filtered data stream.&lt;/P&gt;
&lt;P&gt;For the EXTINT pin, it is an input pin, which can accept external signal to fire interrupt.&lt;/P&gt;
&lt;P&gt;If I misunderstand you, I am sorry.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Wed, 16 Mar 2022 02:16:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/lpc1768-EXTINT-interface/m-p/1428882#M48239</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-03-16T02:16:12Z</dc:date>
    </item>
    <item>
      <title>Re: lpc1768 EXTINT interface</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpc1768-EXTINT-interface/m-p/1428940#M48240</link>
      <description>&lt;P&gt;But EXTINT also use For an Counting purpose&lt;/P&gt;</description>
      <pubDate>Wed, 16 Mar 2022 03:49:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/lpc1768-EXTINT-interface/m-p/1428940#M48240</guid>
      <dc:creator>Sukumar_M</dc:creator>
      <dc:date>2022-03-16T03:49:58Z</dc:date>
    </item>
    <item>
      <title>Re: lpc1768 EXTINT interface</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpc1768-EXTINT-interface/m-p/1429023#M48241</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;If you want to count external clock number, you can connect the external clock signal to the Timer Capx pin, by proper configuration, the Timer will count the number of external clock signal.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Wed, 16 Mar 2022 06:48:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/lpc1768-EXTINT-interface/m-p/1429023#M48241</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-03-16T06:48:20Z</dc:date>
    </item>
  </channel>
</rss>