<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Cursor position LCD display in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Cursor-position-LCD-display/m-p/1425199#M48150</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using an LCD module based on the HD44780, I am using it in 8 bit mode, connecting an external LCD module with the help of jumpers.&lt;/P&gt;&lt;P&gt;I re wrote the code for the display using the same logic, but this time instead of using IOPIN0 register I used IOSET0 and IOCLR0 to control the GPIO PINs and the display is working absolutely fine. Can you please explain the reason for this behavior.&lt;/P&gt;</description>
    <pubDate>Wed, 09 Mar 2022 10:23:41 GMT</pubDate>
    <dc:creator>Arush08</dc:creator>
    <dc:date>2022-03-09T10:23:41Z</dc:date>
    <item>
      <title>Cursor position LCD display</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Cursor-position-LCD-display/m-p/1423420#M48118</link>
      <description>&lt;P&gt;Hi, I am a student who has recently started using LPC2148 Uc, I was interfacing the Uc with a 16X2 LCD display and I am facing certain problems. I am able to print strings on the first row, however I am unsuccessful in printing a string to the second line, I can see the cursor blinking on the second row, however nothing is printing. I tried printing "Hello" from 0x85, the first letter, i.e. H prints at the desire location, however everything after that is printing in the second row in reverse order. I am attaching the code here, can someone please explain what I am doing wrong,&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Fri, 04 Mar 2022 19:25:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Cursor-position-LCD-display/m-p/1423420#M48118</guid>
      <dc:creator>Arush08</dc:creator>
      <dc:date>2022-03-04T19:25:34Z</dc:date>
    </item>
    <item>
      <title>Re: Cursor position LCD display</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Cursor-position-LCD-display/m-p/1423689#M48123</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Can you tell us the part number of your LCD? how do you connect the LCD with the LPC2148?&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Mon, 07 Mar 2022 05:43:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Cursor-position-LCD-display/m-p/1423689#M48123</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-03-07T05:43:24Z</dc:date>
    </item>
    <item>
      <title>Re: Cursor position LCD display</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Cursor-position-LCD-display/m-p/1425199#M48150</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using an LCD module based on the HD44780, I am using it in 8 bit mode, connecting an external LCD module with the help of jumpers.&lt;/P&gt;&lt;P&gt;I re wrote the code for the display using the same logic, but this time instead of using IOPIN0 register I used IOSET0 and IOCLR0 to control the GPIO PINs and the display is working absolutely fine. Can you please explain the reason for this behavior.&lt;/P&gt;</description>
      <pubDate>Wed, 09 Mar 2022 10:23:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Cursor-position-LCD-display/m-p/1425199#M48150</guid>
      <dc:creator>Arush08</dc:creator>
      <dc:date>2022-03-09T10:23:41Z</dc:date>
    </item>
  </channel>
</rss>