<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic UART Bootloader LPC55S16 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/UART-Bootloader-LPC55S16/m-p/1420568#M48060</link>
    <description>&lt;P&gt;Did I understand the table "Table 195. ISP pin assignments" correctly, that a bootloader which uses the UART interface is only usable with Flexcomm0 and i2c only with Flexcomm1? Or can I use UART also with Flexcomm1?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Ralf&lt;/P&gt;</description>
    <pubDate>Mon, 28 Feb 2022 13:03:09 GMT</pubDate>
    <dc:creator>Ralf_Rademacher</dc:creator>
    <dc:date>2022-02-28T13:03:09Z</dc:date>
    <item>
      <title>UART Bootloader LPC55S16</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/UART-Bootloader-LPC55S16/m-p/1420568#M48060</link>
      <description>&lt;P&gt;Did I understand the table "Table 195. ISP pin assignments" correctly, that a bootloader which uses the UART interface is only usable with Flexcomm0 and i2c only with Flexcomm1? Or can I use UART also with Flexcomm1?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Ralf&lt;/P&gt;</description>
      <pubDate>Mon, 28 Feb 2022 13:03:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/UART-Bootloader-LPC55S16/m-p/1420568#M48060</guid>
      <dc:creator>Ralf_Rademacher</dc:creator>
      <dc:date>2022-02-28T13:03:09Z</dc:date>
    </item>
    <item>
      <title>Re: UART Bootloader LPC55S16</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/UART-Bootloader-LPC55S16/m-p/1421365#M48088</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/115185"&gt;@Ralf_Rademacher&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;The ISP boot is available on the following serial interfaces:&lt;/P&gt;
&lt;P&gt;- UART0&lt;/P&gt;
&lt;P&gt;- I2C1&lt;/P&gt;
&lt;P&gt;- SPI3&lt;/P&gt;
&lt;P&gt;- USB0_FS&lt;/P&gt;
&lt;P&gt;- USB1-HS&lt;/P&gt;
&lt;P&gt;So answering your question yes the USART ISP mode is only available on the FC0. Please let me know if you find this information useful.&lt;/P&gt;</description>
      <pubDate>Tue, 01 Mar 2022 18:57:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/UART-Bootloader-LPC55S16/m-p/1421365#M48088</guid>
      <dc:creator>nxf77486</dc:creator>
      <dc:date>2022-03-01T18:57:44Z</dc:date>
    </item>
    <item>
      <title>Re: UART Bootloader LPC55S16</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/UART-Bootloader-LPC55S16/m-p/1425578#M48154</link>
      <description>&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;P&gt;Hi &lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/190340" target="_blank" rel="noopener"&gt;@nxf77486&lt;/A&gt; ,&lt;/P&gt;&lt;P&gt;i think it wasnt the correct answer on what i initially ment. i think what i mean is a secondary bootloader. could it be, that i can use any FC i want for UART there?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Ralf&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Wed, 09 Mar 2022 19:35:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/UART-Bootloader-LPC55S16/m-p/1425578#M48154</guid>
      <dc:creator>Ralf_Rademacher</dc:creator>
      <dc:date>2022-03-09T19:35:20Z</dc:date>
    </item>
  </channel>
</rss>