<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollersのトピックdevice ID on LPC5512</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/device-ID-on-LPC5512/m-p/1411622#M47881</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I try to read the device ID with ISP command through UART, but it can't read out the correct device ID number.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The command I send is:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;BYTE command1[] = {0x5A, 0xA4, 0x0C,0x00,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;0x2C, 0x49, //crc16&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;0x07, //getproperty&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;0x00,0x00,0x02, //2 para&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;0x10,0x00,0x00,0x00, //device id tag 0x10&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;0x00,0x00,0x00,0x00};&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;And the data returned from the device is : 0x5A,0xA4,0x08,0x00,0x92,0x68,0xA7,0x00,0x00,0x01,0x3C,0x28,0x00,0x00.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In the datasheet, the device id for LPC5512 is 0xA100370C, is different with the data I received 0x283C.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;please help to check. &lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;/Jakob&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 10 Feb 2022 07:34:33 GMT</pubDate>
    <dc:creator>JRIIS</dc:creator>
    <dc:date>2022-02-10T07:34:33Z</dc:date>
    <item>
      <title>device ID on LPC5512</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/device-ID-on-LPC5512/m-p/1411622#M47881</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I try to read the device ID with ISP command through UART, but it can't read out the correct device ID number.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The command I send is:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;BYTE command1[] = {0x5A, 0xA4, 0x0C,0x00,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;0x2C, 0x49, //crc16&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;0x07, //getproperty&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;0x00,0x00,0x02, //2 para&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;0x10,0x00,0x00,0x00, //device id tag 0x10&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;0x00,0x00,0x00,0x00};&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;And the data returned from the device is : 0x5A,0xA4,0x08,0x00,0x92,0x68,0xA7,0x00,0x00,0x01,0x3C,0x28,0x00,0x00.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In the datasheet, the device id for LPC5512 is 0xA100370C, is different with the data I received 0x283C.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;please help to check. &lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;/Jakob&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 10 Feb 2022 07:34:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/device-ID-on-LPC5512/m-p/1411622#M47881</guid>
      <dc:creator>JRIIS</dc:creator>
      <dc:date>2022-02-10T07:34:33Z</dc:date>
    </item>
    <item>
      <title>Re: device ID on LPC5512</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/device-ID-on-LPC5512/m-p/1412308#M47890</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;A id="link_12" class="lia-link-navigation lia-page-link lia-user-name-link" href="https://community.nxp.com/t5/user/viewprofilepage/user-id/8452" target="_self" aria-label="View Profile of JRIIS"&gt;&lt;SPAN class=""&gt;JRIIS&lt;/SPAN&gt;&lt;/A&gt;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;LPC551x/0x doesn't support "get-property 0x10", it is a doc issue.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Alice&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 11 Feb 2022 08:21:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/device-ID-on-LPC5512/m-p/1412308#M47890</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2022-02-11T08:21:42Z</dc:date>
    </item>
  </channel>
</rss>