<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC54616J512BD208 firmware update in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54616J512BD208-firmware-update/m-p/1411494#M47872</link>
    <description>&lt;P&gt;Thank you for the quick reply.&lt;/P&gt;&lt;P&gt;FlashMagic looks promising!&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 10 Feb 2022 03:19:21 GMT</pubDate>
    <dc:creator>istvanmate</dc:creator>
    <dc:date>2022-02-10T03:19:21Z</dc:date>
    <item>
      <title>LPC54616J512BD208 firmware update</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54616J512BD208-firmware-update/m-p/1410597#M47856</link>
      <description>&lt;P&gt;I am starting a new design &lt;FONT face="arial,helvetica,sans-serif"&gt;with&lt;/FONT&gt; the&amp;nbsp;&lt;STRONG&gt;&lt;FONT size="4"&gt;LPC54616J512BD208&amp;nbsp;&lt;/FONT&gt;&lt;/STRONG&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;and having a bit of problem figuring out the field (at end user) firmware update process.&amp;nbsp;I want to use one of the serial ports on the &lt;STRONG&gt;LPC54616J512BD208 &lt;/STRONG&gt;to download the new firmware.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;On the hardware side I think I have what I need. I have a USB to Serial Brige IC and I can use the serial flow control bits and some glue logic to reset the &lt;STRONG&gt;LPC54616J512BD208&lt;/STRONG&gt;&lt;STRONG&gt;&amp;nbsp;&lt;/STRONG&gt;and direct the boot process to internal Flash or to the USART.&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;1) According to the User Manual, if &lt;FONT color="#008000"&gt;GPIO_4 is '0',&amp;nbsp;&amp;nbsp;GPIO_5 is '1' and&amp;nbsp;GPIO_6 is '1' &lt;FONT color="#333333"&gt;, the first valid probe message on USART, I2C, or SPI&amp;nbsp;&lt;/FONT&gt;&lt;FONT color="#333333"&gt;locks in that interface. What is this probe message? Is the PC program downloading the hex code sending this message?&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;&lt;FONT color="#008000"&gt;&lt;FONT color="#333333"&gt;2) Is there a simle, no frills PC program (C#, C++, etc..) example to download the hex code through the&amp;nbsp;USART? At the moment I am not concered with a secure download. Just a basic, easy to understand program.&amp;nbsp;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 09 Feb 2022 02:02:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54616J512BD208-firmware-update/m-p/1410597#M47856</guid>
      <dc:creator>istvanmate</dc:creator>
      <dc:date>2022-02-09T02:02:45Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54616J512BD208 firmware update</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54616J512BD208-firmware-update/m-p/1410687#M47858</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;You can use the FlashMagic tools to download application code to on-chip flash via uart in ISP mode by setting up the ISP0(PIO0_4) pin&amp;nbsp; as LOW during/after Reset, you can download FlashMagic tools from the link:&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.flashmagictool.com/" target="_blank"&gt;https://www.flashmagictool.com/&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Xiangjun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 09 Feb 2022 05:47:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54616J512BD208-firmware-update/m-p/1410687#M47858</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-02-09T05:47:08Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54616J512BD208 firmware update</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54616J512BD208-firmware-update/m-p/1411494#M47872</link>
      <description>&lt;P&gt;Thank you for the quick reply.&lt;/P&gt;&lt;P&gt;FlashMagic looks promising!&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 10 Feb 2022 03:19:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54616J512BD208-firmware-update/m-p/1411494#M47872</guid>
      <dc:creator>istvanmate</dc:creator>
      <dc:date>2022-02-10T03:19:21Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54616J512BD208 firmware update</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54616J512BD208-firmware-update/m-p/1586341#M51344</link>
      <description>&lt;P&gt;Are there other tools beside flashmagic to use the ISP features?&lt;BR /&gt;my board is equiped with USB1 for ISP upgrade port.&amp;nbsp; I have a jumpeer for ISP mode at startup.&lt;BR /&gt;But flashmagic does not program my LPC55S69..&amp;nbsp; reading and erasing works fine.&lt;/P&gt;</description>
      <pubDate>Sat, 21 Jan 2023 09:41:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54616J512BD208-firmware-update/m-p/1586341#M51344</guid>
      <dc:creator>MVWare</dc:creator>
      <dc:date>2023-01-21T09:41:48Z</dc:date>
    </item>
  </channel>
</rss>