<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC1768 replacing LPC2368</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-replacing-LPC2368/m-p/1409710#M47840</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;Jun Zhang&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Many thanks, this is the answer i was waiting for !&lt;/P&gt;&lt;P&gt;Have a nice day.&lt;/P&gt;</description>
    <pubDate>Mon, 07 Feb 2022 13:53:44 GMT</pubDate>
    <dc:creator>Savelec</dc:creator>
    <dc:date>2022-02-07T13:53:44Z</dc:date>
    <item>
      <title>LPC1768 replacing LPC2368</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-replacing-LPC2368/m-p/1408050#M47815</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to use the LPC1768 in replacement for the LPC2368 on&amp;nbsp;existing electronic boards.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The pin n°13 on LPC2368 (LQFP100 package) must be connected to Vdd (3.3V) but the pin in "not connected" on LPC1768.&lt;/P&gt;&lt;P&gt;Can I&amp;nbsp;still leave this pin to Vdd on LPC1768 or this pin must be not connected ?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Wed, 02 Feb 2022 14:06:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-replacing-LPC2368/m-p/1408050#M47815</guid>
      <dc:creator>Savelec</dc:creator>
      <dc:date>2022-02-02T14:06:56Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1768 replacing LPC2368</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-replacing-LPC2368/m-p/1409698#M47838</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/196454"&gt;@Savelec&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;the LPC1768 is a replacement for the LPC2368.&lt;/P&gt;
&lt;P&gt;Regarding to the pin, LPC1768 pin13 is nc while LPC2368 connects to Vdd. The LPC1768 and the LPC2368 are not strictly pin-compatible. However it's possible to directly replace a LPC2368 with an LPC1768/66 (at the same board.).In this case it's no problem to connect the NC pin 13 of the LPC1768 to Vdd&lt;/P&gt;
&lt;P&gt;However, please note the longevity of LPC1766/8/9 are less than 5 years left. We don’t have other pin to pin replacement longer than10 years.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope this helps.&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Mon, 07 Feb 2022 13:26:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-replacing-LPC2368/m-p/1409698#M47838</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2022-02-07T13:26:57Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1768 replacing LPC2368</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-replacing-LPC2368/m-p/1409710#M47840</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;Jun Zhang&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Many thanks, this is the answer i was waiting for !&lt;/P&gt;&lt;P&gt;Have a nice day.&lt;/P&gt;</description>
      <pubDate>Mon, 07 Feb 2022 13:53:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-replacing-LPC2368/m-p/1409710#M47840</guid>
      <dc:creator>Savelec</dc:creator>
      <dc:date>2022-02-07T13:53:44Z</dc:date>
    </item>
  </channel>
</rss>