<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SD card with LPC55s69-EVK - Peripherals Tool in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/SD-card-with-LPC55s69-EVK-Peripherals-Tool/m-p/1409348#M47830</link>
    <description>&lt;P&gt;Hey,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm working with the LCP5569-EVK and wish to add an SD card as external memory.&lt;BR /&gt;I've looked through the demo code and it seems pretty straight forward.&lt;BR /&gt;I was wondering if its possible to set up the SD in MCUexpressos peripherals tool as I've done with SPI etc.&lt;BR /&gt;&lt;BR /&gt;Kind regards,&amp;nbsp;&lt;BR /&gt;Lexi&lt;/P&gt;</description>
    <pubDate>Mon, 07 Feb 2022 02:41:37 GMT</pubDate>
    <dc:creator>BabyBorisova</dc:creator>
    <dc:date>2022-02-07T02:41:37Z</dc:date>
    <item>
      <title>SD card with LPC55s69-EVK - Peripherals Tool</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SD-card-with-LPC55s69-EVK-Peripherals-Tool/m-p/1409348#M47830</link>
      <description>&lt;P&gt;Hey,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm working with the LCP5569-EVK and wish to add an SD card as external memory.&lt;BR /&gt;I've looked through the demo code and it seems pretty straight forward.&lt;BR /&gt;I was wondering if its possible to set up the SD in MCUexpressos peripherals tool as I've done with SPI etc.&lt;BR /&gt;&lt;BR /&gt;Kind regards,&amp;nbsp;&lt;BR /&gt;Lexi&lt;/P&gt;</description>
      <pubDate>Mon, 07 Feb 2022 02:41:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SD-card-with-LPC55s69-EVK-Peripherals-Tool/m-p/1409348#M47830</guid>
      <dc:creator>BabyBorisova</dc:creator>
      <dc:date>2022-02-07T02:41:37Z</dc:date>
    </item>
    <item>
      <title>Re: SD card with LPC55s69-EVK - Peripherals Tool</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SD-card-with-LPC55s69-EVK-Peripherals-Tool/m-p/1409602#M47835</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&amp;nbsp;&lt;SPAN&gt;BabyBorisova,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;There is SD card demo under SDK, you can have a look, download from:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://mcuxpresso.nxp.com/en/select" target="_blank"&gt;https://mcuxpresso.nxp.com/en/select&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Mon, 07 Feb 2022 10:10:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SD-card-with-LPC55s69-EVK-Peripherals-Tool/m-p/1409602#M47835</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2022-02-07T10:10:54Z</dc:date>
    </item>
  </channel>
</rss>