<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックWant to differentiate Two LPCXpresso54120 Bridge devices.</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Want-to-differentiate-Two-LPCXpresso54120-Bridge-devices/m-p/1406643#M47778</link>
    <description>&lt;P&gt;We have LPCXpresso54102 LQFP64 Rev A board. we use this board as USB to I2C bridge. We use LIBUSBSIO python library for I2C operation of Bridge.&lt;/P&gt;&lt;P&gt;Now, We have these 2 bridges connected with the PC and we want to differentiate the device.&lt;/P&gt;&lt;P&gt;sio = LIBUSBSIO(loglevel=logging.DEBUG)&lt;BR /&gt;numports = sio.GetNumPorts()&lt;/P&gt;&lt;P&gt;sio.Open(0)&lt;/P&gt;&lt;P&gt;here sio.GetNumPorts() give no of connected sio device. for the Opening port we just give no of a device(In my case 0 or 1).so, how can we identify which board is comport is open?&lt;/P&gt;&lt;P&gt;There is any way to find which device is open.&lt;BR /&gt;Please suggest to me some ideas related to my usage?&lt;/P&gt;</description>
    <pubDate>Fri, 28 Jan 2022 13:51:02 GMT</pubDate>
    <dc:creator>Harshal_Kaswala</dc:creator>
    <dc:date>2022-01-28T13:51:02Z</dc:date>
    <item>
      <title>Want to differentiate Two LPCXpresso54120 Bridge devices.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Want-to-differentiate-Two-LPCXpresso54120-Bridge-devices/m-p/1406643#M47778</link>
      <description>&lt;P&gt;We have LPCXpresso54102 LQFP64 Rev A board. we use this board as USB to I2C bridge. We use LIBUSBSIO python library for I2C operation of Bridge.&lt;/P&gt;&lt;P&gt;Now, We have these 2 bridges connected with the PC and we want to differentiate the device.&lt;/P&gt;&lt;P&gt;sio = LIBUSBSIO(loglevel=logging.DEBUG)&lt;BR /&gt;numports = sio.GetNumPorts()&lt;/P&gt;&lt;P&gt;sio.Open(0)&lt;/P&gt;&lt;P&gt;here sio.GetNumPorts() give no of connected sio device. for the Opening port we just give no of a device(In my case 0 or 1).so, how can we identify which board is comport is open?&lt;/P&gt;&lt;P&gt;There is any way to find which device is open.&lt;BR /&gt;Please suggest to me some ideas related to my usage?&lt;/P&gt;</description>
      <pubDate>Fri, 28 Jan 2022 13:51:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Want-to-differentiate-Two-LPCXpresso54120-Bridge-devices/m-p/1406643#M47778</guid>
      <dc:creator>Harshal_Kaswala</dc:creator>
      <dc:date>2022-01-28T13:51:02Z</dc:date>
    </item>
    <item>
      <title>Re: Want to differentiate Two LPCXpresso54120 Bridge devices.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Want-to-differentiate-Two-LPCXpresso54120-Bridge-devices/m-p/1412232#M47888</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Multiple LPC controller targets can be attached to the host. The current version of the library doesn’t&lt;BR /&gt;provide a mechanism to uniquely identify individual targets except with an index number (starting from&lt;BR /&gt;zero) assigned during enumeration.&lt;/P&gt;
&lt;P&gt;For more, please see attached manual&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Fri, 11 Feb 2022 06:28:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Want-to-differentiate-Two-LPCXpresso54120-Bridge-devices/m-p/1412232#M47888</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2022-02-11T06:28:15Z</dc:date>
    </item>
  </channel>
</rss>