<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC55S69 CASPER performances detail</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-CASPER-performances-detail/m-p/1404355#M47739</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;As you know that the LPC55xx has on-chip flash and on-chip RAM, both the on-chip Flash and RAM can be used to save application code and run from them directly. The LPC55S69 for example can run at 150mhz, but reading/executing&amp;nbsp; code from flash requires delay clock, which can be set with the FLASHTIM bits in FMC configuration register. But If you run in on-chip SRAM, delay is not needed, so running in on-chip SRAM is faster than that of running in on-chip flash. user can copy code application code from flash to SRAM and execute in SRAM directly.&lt;/P&gt;
&lt;P&gt;For the memory map, pls refer to Chapter 2: LPC55S6x/LPC55S2x/LPC552x Memory Map in UM11126.pdf&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1643092629441.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/168736iFFCFE7F154A160FB/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1643092629441.png" alt="xiangjun_rong_0-1643092629441.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;xiangjun_rong_0-1643092629441.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 25 Jan 2022 06:43:03 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2022-01-25T06:43:03Z</dc:date>
    <item>
      <title>LPC55S69 CASPER performances detail</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-CASPER-performances-detail/m-p/1404123#M47735</link>
      <description>&lt;P&gt;Hi, In the AN12445 rev. 4, 10/2020, the performances of Figure 8 are illustrated with the columns titles "Flash" and "RAM". I have found no details of what the "Flash" and "RAM" columns mean. Could you please provide an explanation on their difference? Do the SDK allows achieving Flash or RAM performances?&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;AB&lt;/P&gt;</description>
      <pubDate>Mon, 24 Jan 2022 18:18:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-CASPER-performances-detail/m-p/1404123#M47735</guid>
      <dc:creator>albertobattistello</dc:creator>
      <dc:date>2022-01-24T18:18:38Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69 CASPER performances detail</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-CASPER-performances-detail/m-p/1404355#M47739</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;As you know that the LPC55xx has on-chip flash and on-chip RAM, both the on-chip Flash and RAM can be used to save application code and run from them directly. The LPC55S69 for example can run at 150mhz, but reading/executing&amp;nbsp; code from flash requires delay clock, which can be set with the FLASHTIM bits in FMC configuration register. But If you run in on-chip SRAM, delay is not needed, so running in on-chip SRAM is faster than that of running in on-chip flash. user can copy code application code from flash to SRAM and execute in SRAM directly.&lt;/P&gt;
&lt;P&gt;For the memory map, pls refer to Chapter 2: LPC55S6x/LPC55S2x/LPC552x Memory Map in UM11126.pdf&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1643092629441.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/168736iFFCFE7F154A160FB/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1643092629441.png" alt="xiangjun_rong_0-1643092629441.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;xiangjun_rong_0-1643092629441.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jan 2022 06:43:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-CASPER-performances-detail/m-p/1404355#M47739</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-01-25T06:43:03Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69 CASPER performances detail</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-CASPER-performances-detail/m-p/1404604#M47744</link>
      <description>&lt;P&gt;Thank you very much for your fast response.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;AB&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jan 2022 14:37:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-CASPER-performances-detail/m-p/1404604#M47744</guid>
      <dc:creator>albertobattistello</dc:creator>
      <dc:date>2022-01-25T14:37:11Z</dc:date>
    </item>
  </channel>
</rss>