<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC15xx - Pull-up disable when configured as ADC</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC15xx-Pull-up-disable-when-configured-as-ADC/m-p/1402855#M47703</link>
    <description>&lt;P&gt;From LPC15xx device user manual (UM10736):&lt;/P&gt;&lt;P&gt;From Section 7.4.5:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;When using a pin in analog mode, disable the pull-up and pull-down resistors.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;From Section 7.5.1&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;If any of the pins is connected to an analog function through the switch matrix&lt;BR /&gt;PINENABLE registers, the digital portion of the pin is disconnected.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;These two statements appear to contradict each other.&lt;/P&gt;&lt;P&gt;Do the pull-up resistors remain connected when the pin is configured as an ADC pin?&amp;nbsp; If not, please confirm that the pull-up resistor need not be disabled, as suggested above, when configuring as an ADC.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Jonathon&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 20 Jan 2022 20:07:10 GMT</pubDate>
    <dc:creator>jonathon_generac</dc:creator>
    <dc:date>2022-01-20T20:07:10Z</dc:date>
    <item>
      <title>LPC15xx - Pull-up disable when configured as ADC</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC15xx-Pull-up-disable-when-configured-as-ADC/m-p/1402855#M47703</link>
      <description>&lt;P&gt;From LPC15xx device user manual (UM10736):&lt;/P&gt;&lt;P&gt;From Section 7.4.5:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;When using a pin in analog mode, disable the pull-up and pull-down resistors.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;From Section 7.5.1&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;If any of the pins is connected to an analog function through the switch matrix&lt;BR /&gt;PINENABLE registers, the digital portion of the pin is disconnected.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;These two statements appear to contradict each other.&lt;/P&gt;&lt;P&gt;Do the pull-up resistors remain connected when the pin is configured as an ADC pin?&amp;nbsp; If not, please confirm that the pull-up resistor need not be disabled, as suggested above, when configuring as an ADC.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Jonathon&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 20 Jan 2022 20:07:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC15xx-Pull-up-disable-when-configured-as-ADC/m-p/1402855#M47703</guid>
      <dc:creator>jonathon_generac</dc:creator>
      <dc:date>2022-01-20T20:07:10Z</dc:date>
    </item>
    <item>
      <title>Re: LPC15xx - Pull-up disable when configured as ADC</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC15xx-Pull-up-disable-when-configured-as-ADC/m-p/1402929#M47705</link>
      <description>&lt;P&gt;Hi, Jonathon,&lt;/P&gt;
&lt;P&gt;Regarding your question, pls refer to section 7.4.1 pin configuration in UM10736.pdf, you can see that the week pull-up and pull-down circuit is an independent circuit, belongs to IOCON module, you have to disable the both weak pull-up and pull-down so that the ADC sample is not effected by the pull-up and pull-down circuit.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_1-1642726322446.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/168426i7E3BBED2EEBD8C13/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_1-1642726322446.png" alt="xiangjun_rong_1-1642726322446.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1642725988134.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/168425i9163E8BDB706C204/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1642725988134.png" alt="xiangjun_rong_0-1642725988134.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 21 Jan 2022 00:56:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC15xx-Pull-up-disable-when-configured-as-ADC/m-p/1402929#M47705</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-01-21T00:56:38Z</dc:date>
    </item>
  </channel>
</rss>